<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC 1857 EEPROM error</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1857-EEPROM-error/m-p/1293606#M45500</link>
    <description>&lt;P lang="es-MX"&gt;Hello&lt;/P&gt;
&lt;P lang="es-MX"&gt;Hope you´re well. &lt;BR /&gt;The wait values of the LPCOpen are correct. However you can change these parameters if you think they will give better results. &lt;BR /&gt;&lt;BR /&gt;Let me know if you have further questions. &lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 16 Jun 2021 21:59:25 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2021-06-16T21:59:25Z</dc:date>
    <item>
      <title>LPC 1857 EEPROM error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1857-EEPROM-error/m-p/1290502#M45401</link>
      <description>&lt;P&gt;I'm using internal EEPROM of an LPC1857 having internal sysclock&amp;nbsp;@ 180 MHz, sometimes errors occurr reading or writing the EEPROM (the read write operations are always dword aligned).&lt;/P&gt;&lt;P&gt;Checking the EEPROM initialization of read and write wait cycles I found the following values&lt;/P&gt;&lt;P&gt;#define EEPROM_READ_WAIT_STATE_VAL&amp;nbsp; &amp;nbsp; 0x58&lt;BR /&gt;#define EEPROM_WAIT_STATE_VAL&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 0x232&lt;/P&gt;&lt;P&gt;but, reading the datasheet of the Processor and calculating the values, I obtain different values.&lt;/P&gt;&lt;P&gt;Question: the values in the file eeprom_18xx_43xx.h of LPCOpen are correct or have to be recalculated for the different custom boards ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 07:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1857-EEPROM-error/m-p/1290502#M45401</guid>
      <dc:creator>luciano_mortari</dc:creator>
      <dc:date>2021-06-10T07:13:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 1857 EEPROM error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1857-EEPROM-error/m-p/1293606#M45500</link>
      <description>&lt;P lang="es-MX"&gt;Hello&lt;/P&gt;
&lt;P lang="es-MX"&gt;Hope you´re well. &lt;BR /&gt;The wait values of the LPCOpen are correct. However you can change these parameters if you think they will give better results. &lt;BR /&gt;&lt;BR /&gt;Let me know if you have further questions. &lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jun 2021 21:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1857-EEPROM-error/m-p/1293606#M45500</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-06-16T21:59:25Z</dc:date>
    </item>
  </channel>
</rss>