<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DCDC LPC55S14 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1291231#M45433</link>
    <description>&lt;P&gt;Hello to all.&lt;/P&gt;&lt;P&gt;I am using for the first time the LPC55S14 microcontroller, I can't find much information about the DCDC converter, if someone could tell me where I can find more information. I already read the datasheet and the user manual, but I can't find much information.&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;Can this converter be used to power the microphone itself? If so, what would the hardware connections be like?&lt;BR /&gt;If it can't be used for this, what would be the connections to the micro so as not to use the dcdc?&lt;/P&gt;&lt;P&gt;Thank you very much. Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 11 Jun 2021 08:43:31 GMT</pubDate>
    <dc:creator>Nadia</dc:creator>
    <dc:date>2021-06-11T08:43:31Z</dc:date>
    <item>
      <title>DCDC LPC55S14</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1291231#M45433</link>
      <description>&lt;P&gt;Hello to all.&lt;/P&gt;&lt;P&gt;I am using for the first time the LPC55S14 microcontroller, I can't find much information about the DCDC converter, if someone could tell me where I can find more information. I already read the datasheet and the user manual, but I can't find much information.&lt;/P&gt;&lt;P&gt;My questions are:&lt;/P&gt;&lt;P&gt;Can this converter be used to power the microphone itself? If so, what would the hardware connections be like?&lt;BR /&gt;If it can't be used for this, what would be the connections to the micro so as not to use the dcdc?&lt;/P&gt;&lt;P&gt;Thank you very much. Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 08:43:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1291231#M45433</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-06-11T08:43:31Z</dc:date>
    </item>
    <item>
      <title>Re: DCDC LPC55S14</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1292202#M45465</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181156" target="_self" aria-label="View Profile of Nadia"&gt;&lt;SPAN class=""&gt;Nadia&lt;/SPAN&gt;&lt;/A&gt;,&lt;/P&gt;
&lt;P&gt;There is an application note about LPC55xx DCDC, you can have a look:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12325.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12325.pdf&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jun 2021 02:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1292202#M45465</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-06-15T02:53:39Z</dc:date>
    </item>
    <item>
      <title>Re: DCDC LPC55S14</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1309048#M45880</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'd like to know what the expected output voltage of the internal DCDC converter of the LPC55xx is, see red circled node in the screenshot below (copied from AN12325, page 2)?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="danielholala_0-1626429127607.png" style="width: 725px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150061i04BB712695C8F58D/image-dimensions/725x433?v=v2" width="725" height="433" role="button" title="danielholala_0-1626429127607.png" alt="danielholala_0-1626429127607.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielholala_0-1626429127607.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;That is, what voltage is at VDD_PMU typically? I know that according to the datasheet, VDD_PMU maximum voltage is 1.26 V. So the output node of the DCDC converter will be below this voltage. But what should I expect? 1.0 V? I'm designing my own custom board using LPC5526 and I'd like to verify that it is working properly.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jul 2021 09:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1309048#M45880</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2021-07-16T09:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: DCDC LPC55S14</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1451314#M48608</link>
      <description>&lt;P&gt;I don't want to use the DCDC converter. What must I do with these pins if they're not being used?&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 11:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DCDC-LPC55S14/m-p/1451314#M48608</guid>
      <dc:creator>cwouse</dc:creator>
      <dc:date>2022-04-29T11:55:41Z</dc:date>
    </item>
  </channel>
</rss>