<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1114FBD48/301 - replacement in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1291133#M45428</link>
    <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;We don't use these functions in our code and I have to be sure that it will work the same on both types.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;That is, if we do not configure these functions, they have default settings that are identical to the configuration in type ... / 301?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Karol_VT&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 11 Jun 2021 06:46:59 GMT</pubDate>
    <dc:creator>Karol_VT</dc:creator>
    <dc:date>2021-06-11T06:46:59Z</dc:date>
    <item>
      <title>LPC1114FBD48/301 - replacement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1290919#M45418</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using LPC1114FBD48/301.&lt;/P&gt;&lt;P&gt;Now due to a problem with availability of this type we want to use LPC1114FBD48/302 interchangeably.&lt;/P&gt;&lt;P&gt;Please let me know if the code writen for&amp;nbsp;LPC1114FBD48/301 will work the same on the type&amp;nbsp;LPC1114FBD48/302 ?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Karol&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 21:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1290919#M45418</guid>
      <dc:creator>Karol_VT</dc:creator>
      <dc:date>2021-06-10T21:02:26Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114FBD48/301 - replacement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1290984#M45423</link>
      <description>&lt;P&gt;Hi, Karol,&lt;/P&gt;
&lt;P&gt;I think that the LPC1114FBD48/302 and LPC1114FBD48/301 can be used interchangeably.&lt;/P&gt;
&lt;P&gt;Regarding the difference between LPC1114FBD48/302 and LPC1114FBD48/301, first of all, they have the same pin assignment, same peripherals, the only difference is the power profiles, in other words, the ROM code is different.&lt;/P&gt;
&lt;P&gt;The LPC1114FBD48/302 belongs to LPC1100L series, only the LPC1100L series has the power profiles, it provides two ROM api&amp;nbsp; functions: set_pll() and set_power().&lt;/P&gt;
&lt;P&gt;For detailed inf, pls refer to Chapter 5: LPC111x/LPC11Cxx Power profiles in UM10398.pdf.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1623374239192.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146855i35AFF1A76368D046/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1623374239192.png" alt="xiangjun_rong_0-1623374239192.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 01:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1290984#M45423</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-06-11T01:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114FBD48/301 - replacement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1291133#M45428</link>
      <description>&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;We don't use these functions in our code and I have to be sure that it will work the same on both types.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;That is, if we do not configure these functions, they have default settings that are identical to the configuration in type ... / 301?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;Karol_VT&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 06:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1291133#M45428</guid>
      <dc:creator>Karol_VT</dc:creator>
      <dc:date>2021-06-11T06:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1114FBD48/301 - replacement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1291214#M45430</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;As I said that the LPC1114FBD48/302 and LPC1114FBD48/301 can be used interchangeably, because only ROM code is different from software, which you do not call. For the hardware, the&amp;nbsp;LPC1114FBD48/302 support programmable open drain mode which you do not use. so you do not need to change any software or hardware, the LPC1114FBD48/302 and LPC1114FBD48/301 can be exchanged.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_1-1623404535116.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146915iE8B7B7CFF75D383A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_1-1623404535116.png" alt="xiangjun_rong_1-1623404535116.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1623404465238.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146914i538BA4C94DADA5C9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1623404465238.png" alt="xiangjun_rong_0-1623404465238.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jun 2021 09:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1114FBD48-301-replacement/m-p/1291214#M45430</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-06-11T09:45:29Z</dc:date>
    </item>
  </channel>
</rss>