<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55xx :  enter ISP mode with UART in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290461#M45398</link>
    <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;how can I enter in ISP UART mode (without ISP pin)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Have a look at the manual UM11126,&amp;nbsp;chapter 6: "LPC55S6x/LPC55S2x/LPC552x Boot ROM".&lt;/P&gt;&lt;P&gt;There it reads:&lt;/P&gt;&lt;P&gt;&lt;FONT face="book antiqua,palatino"&gt;There are several paths into the ISP mode:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through the ISP pin assertion.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This mechanism is mainly used on EVK boards and customer boards where&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;switches and jumpers are affordable in-terms of space and cost.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This method is used to recover a part programmed with corrupted image which is&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;not detectable by ROM. Once in ISP mode commands are provided to re-program&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;the flash with proper image.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through fall-through mode.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– When the user image in flash is blank or invalid the ROM enters into ISP mode.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This mode of entry allows programming factory fresh parts through ISP interface.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through ROM API call.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– Used by application code to implement in field update using ISP mechanism&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through the Debug Mailbox command.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This mechanism is mainly used to recover a part programmed with a corrupted image. For instance, on boards/products where the ISP pin mechanism in not affordable and SED pins are accessible or when ISP mode is disabled through the “Default ISP mode” field in the CMPA_BOOT_CFG configuration word.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– For security sensitive application option to control access to this mechanism is provided through Debug Authentication procedure.&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Thu, 10 Jun 2021 06:20:23 GMT</pubDate>
    <dc:creator>danielholala</dc:creator>
    <dc:date>2021-06-10T06:20:23Z</dc:date>
    <item>
      <title>LPC55xx :  enter ISP mode with UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1289963#M45376</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to enter ISP mode with UART (flexcom 0)&lt;/P&gt;&lt;P&gt;Is it possible when a firmware is already in place on LPC55xx ?&lt;/P&gt;&lt;P&gt;After a reset, I send a "ping" command (5A A6), but I receive no response and the program in place launch.&lt;/P&gt;&lt;P&gt;The default CMPA is in "Auto ISP" mode&lt;/P&gt;&lt;P&gt;How to force CMPA to be in "UART ISP" mode without ISP pin ?&lt;/P&gt;&lt;P&gt;Note : When LPC55xx have no firmware, the "ping" command have a response ACK (5A A7 ...), because the LPC55xx goes into ISP mode automatically&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Phil&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 15:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1289963#M45376</guid>
      <dc:creator>Phil49</dc:creator>
      <dc:date>2021-06-09T15:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx :  enter ISP mode with UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290391#M45395</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;When the user image in flash is blank or invalid, it will enter ISP mode refer to&amp;nbsp;DEFAULT_ISP_MODE bits defined in Table 170.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1623296466430.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146782iB808D9E8841C5CD1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1623296466430.png" alt="Alice_Yang_0-1623296466430.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1623296466430.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is meaning, if there is a work well image in flash, it won't check&amp;nbsp;DEFAULT_ISP_MODE bits.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 03:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290391#M45395</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-06-10T03:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx :  enter ISP mode with UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290427#M45397</link>
      <description>&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;So how can I enter in ISP UART mode (without ISP pin) when I want upgrade my firmware ?&lt;/P&gt;&lt;P&gt;Phil&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 05:30:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290427#M45397</guid>
      <dc:creator>Phil49</dc:creator>
      <dc:date>2021-06-10T05:30:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx :  enter ISP mode with UART</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290461#M45398</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;how can I enter in ISP UART mode (without ISP pin)&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Have a look at the manual UM11126,&amp;nbsp;chapter 6: "LPC55S6x/LPC55S2x/LPC552x Boot ROM".&lt;/P&gt;&lt;P&gt;There it reads:&lt;/P&gt;&lt;P&gt;&lt;FONT face="book antiqua,palatino"&gt;There are several paths into the ISP mode:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through the ISP pin assertion.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This mechanism is mainly used on EVK boards and customer boards where&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;switches and jumpers are affordable in-terms of space and cost.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This method is used to recover a part programmed with corrupted image which is&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;not detectable by ROM. Once in ISP mode commands are provided to re-program&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;the flash with proper image.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through fall-through mode.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– When the user image in flash is blank or invalid the ROM enters into ISP mode.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This mode of entry allows programming factory fresh parts through ISP interface.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through ROM API call.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– Used by application code to implement in field update using ISP mechanism&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT face="book antiqua,palatino"&gt;Entry through the Debug Mailbox command.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– This mechanism is mainly used to recover a part programmed with a corrupted image. For instance, on boards/products where the ISP pin mechanism in not affordable and SED pins are accessible or when ISP mode is disabled through the “Default ISP mode” field in the CMPA_BOOT_CFG configuration word.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="book antiqua,palatino"&gt;– For security sensitive application option to control access to this mechanism is provided through Debug Authentication procedure.&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Thu, 10 Jun 2021 06:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-enter-ISP-mode-with-UART/m-p/1290461#M45398</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2021-06-10T06:20:23Z</dc:date>
    </item>
  </channel>
</rss>