<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Code Doesn't Run After Stopping Debug</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289927#M45372</link>
    <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have run into an issue with my LCP55S06-EVK board. While I have my board plugged up to my computer, I can build and debug my code, and my board runs the code perfectly. However, as soon as a stop the debug, my board stops running the code. It's as if if just gets stuck in the state in which it was when I stopped the debug. Also, upon unplugging my board from the computer and plugging it back in, the code does not run at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is a very frustrating problem, and I would appreciate any help.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 13:19:03 GMT</pubDate>
    <dc:creator>caden013</dc:creator>
    <dc:date>2021-06-09T13:19:03Z</dc:date>
    <item>
      <title>Code Doesn't Run After Stopping Debug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289927#M45372</link>
      <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have run into an issue with my LCP55S06-EVK board. While I have my board plugged up to my computer, I can build and debug my code, and my board runs the code perfectly. However, as soon as a stop the debug, my board stops running the code. It's as if if just gets stuck in the state in which it was when I stopped the debug. Also, upon unplugging my board from the computer and plugging it back in, the code does not run at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is a very frustrating problem, and I would appreciate any help.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 13:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289927#M45372</guid>
      <dc:creator>caden013</dc:creator>
      <dc:date>2021-06-09T13:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: Code Doesn't Run After Stopping Debug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289931#M45373</link>
      <description>&lt;P&gt;Does you code use semihosting? If so, you need a debugger attached for it to run. See these FAQs&lt;/P&gt;&lt;P&gt;&lt;A href="https://guest.eu.guestline.app/DUMBLETON?reservationNumber=BK001555/1&amp;amp;familyName=Morris" target="_blank"&gt;https://guest.eu.guestline.app/DUMBLETON?reservationNumber=BK001555/1&amp;amp;familyName=Morris&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/What-are-none-nohost-and-semihost-libraries/m-p/475327" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/What-are-none-nohost-and-semihost-libraries/m-p/475327&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 13:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289931#M45373</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-06-09T13:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: Code Doesn't Run After Stopping Debug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289936#M45374</link>
      <description>&lt;P&gt;Thanks for the solution! I had to use the NewLib (semihost).&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 13:47:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Code-Doesn-t-Run-After-Stopping-Debug/m-p/1289936#M45374</guid>
      <dc:creator>caden013</dc:creator>
      <dc:date>2021-06-09T13:47:17Z</dc:date>
    </item>
  </channel>
</rss>