<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックADC convValue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-convValue/m-p/1288395#M45332</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am trying to take in analog signal inputs in my board (LPC55S06-EVK). Right now I am running the example code lpadc_interrupt.c provided by NXP. I have Pin 8 of J13 (P0_23/ARD_ADC0_P) connected to Pin 6 of J9 (AVDD), and yet my code gives me this result: "ADC value: 0" which obviously is incorrect. With an input of AVDD, shouldn't the result be 65535?&lt;/P&gt;&lt;P&gt;I have discovered that the variable convValue ultimately gets its value from the "RESFIFO" ADC data result FIFO register; however, no matter how I hook up the wires, I always receive "ADC value: 0."&lt;/P&gt;&lt;P&gt;If someone could help, I would greatly appreciate it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jun 2021 15:02:34 GMT</pubDate>
    <dc:creator>caden013</dc:creator>
    <dc:date>2021-06-07T15:02:34Z</dc:date>
    <item>
      <title>ADC convValue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-convValue/m-p/1288395#M45332</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am trying to take in analog signal inputs in my board (LPC55S06-EVK). Right now I am running the example code lpadc_interrupt.c provided by NXP. I have Pin 8 of J13 (P0_23/ARD_ADC0_P) connected to Pin 6 of J9 (AVDD), and yet my code gives me this result: "ADC value: 0" which obviously is incorrect. With an input of AVDD, shouldn't the result be 65535?&lt;/P&gt;&lt;P&gt;I have discovered that the variable convValue ultimately gets its value from the "RESFIFO" ADC data result FIFO register; however, no matter how I hook up the wires, I always receive "ADC value: 0."&lt;/P&gt;&lt;P&gt;If someone could help, I would greatly appreciate it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 15:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-convValue/m-p/1288395#M45332</guid>
      <dc:creator>caden013</dc:creator>
      <dc:date>2021-06-07T15:02:34Z</dc:date>
    </item>
    <item>
      <title>Re: ADC convValue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-convValue/m-p/1289601#M45365</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;This is the result I run the lpadc_interrupt example in SDK package.&lt;/P&gt;
&lt;P&gt;I have connected the ADC0_0(pin8 of J13 on LPC55S06-EVK ) to GND or 3.3V, this is the result.&lt;/P&gt;
&lt;P&gt;If you want to use uart to display message as following, you have to close JP12.&lt;/P&gt;
&lt;P&gt;In conclusion, no problem for the lpadc example in SDK package&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1623215990019.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146671iE4E3A57859BDB666/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1623215990019.png" alt="xiangjun_rong_0-1623215990019.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1623215990019.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 05:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-convValue/m-p/1289601#M45365</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-06-09T05:23:32Z</dc:date>
    </item>
  </channel>
</rss>