<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC11e68 - can't read GPIO 0-12 or 0-13</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287117#M45276</link>
    <description>&lt;P&gt;Wouldn't you know that after a week pulling out my hair, I'd figure it out thirty seconds after begging for help?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IOCON_DIGMODE_EN&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Interestingly, that doesn't show up as a configuration in the debugger. IOCON register view.&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jun 2021 01:03:27 GMT</pubDate>
    <dc:creator>chrispflieger</dc:creator>
    <dc:date>2021-06-04T01:03:27Z</dc:date>
    <item>
      <title>LPC11e68 - can't read GPIO 0-12 or 0-13</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287098#M45275</link>
      <description>&lt;P&gt;This seems so simple yet nothing works...&lt;/P&gt;&lt;P&gt;I really need 0-12 to feed a capture timer, but let's just verify these can read the pin state.&lt;/P&gt;&lt;P&gt;IOCON - set to function 1 (because 0 is JTAG). Verified by looking at the registers in the debugger.&lt;/P&gt;&lt;P&gt;The pullup / pulldown function WORKS! - verified with a scope.&lt;/P&gt;&lt;P&gt;Yet the pin value (checked in the&amp;nbsp; GPIO-PORT registers via the debugger) is always zero.&lt;/P&gt;&lt;P&gt;Also I verified the LED functions do work (I can revers the logic and the lights stay on).&lt;/P&gt;&lt;P&gt;In the debugger, I was messing around, and found out that changing the "inverted" mode on the IOCON register would actually turn my LED on and off, changing the pullup doesn't do anything but change the actual pin voltage. It's like it's somehow disconnected inside.&lt;/P&gt;&lt;P&gt;I just can't figure out what I missing here. It's so simple, yet so broken.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;int main(void)
{
    SystemCoreClockUpdate();

    Chip_GPIO_Init(LPC_GPIO);
    Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);

    GREEN_LED_SETUP();
    GREEN_LED_OFF();
    BLUE_LED_SETUP();
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, 0, 12); // reduntant, but testing
    Chip_GPIO_SetPinDIRInput(LPC_GPIO, 0, 13);
    Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 12, IOCON_FUNC1 | IOCON_MODE_PULLDOWN);
    Chip_IOCON_PinMuxSet(LPC_IOCON, 0, 13, IOCON_FUNC1 | IOCON_MODE_PULLDOWN);
    while(1)
    {
        if (Chip_GPIO_ReadPortBit(LPC_GPIO, 0, 13))
        {
            BLUE_LED_ON();
        }
        else
        {
            BLUE_LED_OFF();
        }
        if (Chip_GPIO_ReadPortBit(LPC_GPIO, 0, 12))
        {
            GREEN_LED_ON();
        }
        else
        {
            GREEN_LED_OFF();
        }
    }
}&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I noted that the IOCON table also lists function 5 as having the same property as function 1, but the pullups didn't work for that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did check with another design of ours on this MCU, and it looks like it was using 0-12 for an ADC input OK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 00:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287098#M45275</guid>
      <dc:creator>chrispflieger</dc:creator>
      <dc:date>2021-06-04T00:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11e68 - can't read GPIO 0-12 or 0-13</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287117#M45276</link>
      <description>&lt;P&gt;Wouldn't you know that after a week pulling out my hair, I'd figure it out thirty seconds after begging for help?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IOCON_DIGMODE_EN&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Interestingly, that doesn't show up as a configuration in the debugger. IOCON register view.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 01:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287117#M45276</guid>
      <dc:creator>chrispflieger</dc:creator>
      <dc:date>2021-06-04T01:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11e68 - can't read GPIO 0-12 or 0-13</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287168#M45278</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;From your description, I see that your LED can not work. For the issue, as you know if you want to turn on or turn off a LED, I suppose that you connect the LED to a GPIO pin via a serial resistor. In the case, the pin has to be a output pin instead of an input pin. If the pin is in input mode, the input impedance is several Mohm level, the pin has not enough driving capability to light a lED. In output mode, the pin has several mA driving capability, so the output mode of GPIO pin is required.&lt;/P&gt;
&lt;P&gt;This is a procedure to configure a GPIO pin as output mode.&lt;/P&gt;
&lt;P&gt;1)enable gated clock for the IOCON and the GPIO group&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);&lt;/LI-CODE&gt;
&lt;P&gt;use the similar line to enable the GPIO group gated clock&lt;/P&gt;
&lt;P&gt;2)configure the pin as GPIO function&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;Chip_IOCON_PinMuxSet(LPC_IOCON, 0, LED pin, IOCON_FUNC0 | IOCON_MODE_PULLDOWN);&lt;/LI-CODE&gt;
&lt;P&gt;pls add a option to select digital mode for the above line&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3)configure the pin as GPIO output mode instead of input mode&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;Chip_GPIO_SetPinDIROutput(LPC_GPIO, 0, LED pin);&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;4)toggle the LED pin&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;BLUE_LED_ON();&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;delay()(&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;BLUE_LED_OFF();&lt;/LI-CODE&gt;
&lt;P&gt;delay()&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 02:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11e68-can-t-read-GPIO-0-12-or-0-13/m-p/1287168#M45278</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-06-04T02:35:51Z</dc:date>
    </item>
  </channel>
</rss>