<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286367#M45264</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well. I will gladly help you with this.&lt;BR /&gt;No additional HW is needed. Regarding the software I suggest the SDK; In the SDK you will find the drivers and examples to run the module: &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I suggest you use MCUXpresso IDE with LPC56428 SDK. The examples in the SDK are very helpful and can be used as starting point.&amp;nbsp; &lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jun 2021 22:34:36 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2021-06-02T22:34:36Z</dc:date>
    <item>
      <title>CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286139#M45259</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;i have a question - and in the beginning i say sorry if i ask dumb questions. I am new to Micro Controllers and to the NXP Community/products also. But i want to learn - please be indulgent &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Scenario:&lt;/P&gt;&lt;P&gt;I want to create a little CAN-FD simulation which is sending constant messages into an existing bus system (IDs are known and Datarate is 2Mbits). With buttons i want to change one or two values during power on.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With Google i found the combination of&amp;nbsp;LPCXpresso54628 and OM13099 to get my plan running.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So my question: Do i need an additional HW or SW to get this running or better - what else do i need here?&lt;/P&gt;&lt;P&gt;A subjective question: Do you think for somebody like me it is doable or is it too difficult? I have not that much experience with coding but CAN and electronics i know very good.&lt;/P&gt;&lt;P&gt;Which IDE i should use best here? The NXP SDK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance for your help,&lt;/P&gt;&lt;P&gt;Neolinga&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 13:38:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286139#M45259</guid>
      <dc:creator>Neolinga</dc:creator>
      <dc:date>2021-06-02T13:38:00Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286367#M45264</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well. I will gladly help you with this.&lt;BR /&gt;No additional HW is needed. Regarding the software I suggest the SDK; In the SDK you will find the drivers and examples to run the module: &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I suggest you use MCUXpresso IDE with LPC56428 SDK. The examples in the SDK are very helpful and can be used as starting point.&amp;nbsp; &lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE" target="_blank"&gt;https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 22:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286367#M45264</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-06-02T22:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286818#M45268</link>
      <description>&lt;P&gt;Hello Omar &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;thank you alot for your reply!&lt;/P&gt;&lt;P&gt;Then based on your answer i can order the two products without any risk^^&lt;/P&gt;&lt;P&gt;Firstly i will try to bring it to life on my own. I am using a Vector VN1630 to check the counterpart if messages are recieved. Do i need a separate Debugger/Programmer like ST Link?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If i have questions i will ask it in this post or should i create&amp;nbsp; a specific question? I am doing this for my company and I am not sure if i get it running on my own. Maybe i need the technial support from your side. &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Neolinga&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 12:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1286818#M45268</guid>
      <dc:creator>Neolinga</dc:creator>
      <dc:date>2021-06-03T12:19:58Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1287020#M45270</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;The board is comprised of target LPC54628 device with an onboard, CMSIS-DAP / SEGGER® J-Link compatible debug probe. The onboard probe is compatible with MCUXpresso IDE.&lt;BR /&gt;The board is also equipped with a standard 10-pin header enabling the use of 3rd party to debug probes.&lt;BR /&gt;&lt;BR /&gt;If you have more questions you can post a question in the community or you can submit a ticket: &lt;A href="https://www.nxp.com/support/support:SUPPORTHOME" target="_blank"&gt;https://www.nxp.com/support/support:SUPPORTHOME&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 19:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1287020#M45270</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-06-03T19:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1290755#M45413</link>
      <description>&lt;P&gt;Hello Omar and a good day,&lt;/P&gt;&lt;P&gt;i worked a few days now with the board. I am now more familiar with the IDE and tried a bit with FreeRTOS and GPIOs. Now i tried the Examples from the &lt;A href="https://www.nxp.com/products/interfaces/can-transceivers/can-with-flexible-data-rate/lpcxpresso54618-can-fd-kit:OM13094" target="_self"&gt;OM13094&lt;/A&gt;&amp;nbsp;bottom side (fd_loopback). The CAN-FD Loopback example should transfer the messages from CAN0 to CAN1 and the LEDs should blink. I connected both CANs with a 120Ohm in parallel. (Pin 2/7 on both DSUB sides).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The example displays on Terminal Side (COM side) that no message is transfered and only LED1 on the board blinks permanently.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I dont know what i am doing wrong here. Can you or somebody help me? Debugging/Building everything else worked.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks you a lot for your time and stay healthy&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nils&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 13:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1290755#M45413</guid>
      <dc:creator>Neolinga</dc:creator>
      <dc:date>2021-06-10T13:20:43Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1290927#M45419</link>
      <description>&lt;P&gt;Hello Nils&lt;BR /&gt;&lt;BR /&gt;Hope you are well. I gladly help you with this.&lt;BR /&gt;I suggest you to remove the 120Ohm resistor, the shield already has the necessary components. Also, please make sure that the jumpers JP3,JP4,JP5 and JP6 are connected.&lt;BR /&gt;To install the Shield board, carefully align the J1 pin 1 of the Shield board with J9 pin 1 of the LPCXpresso board, and J3 pin 1 of the Shield board with J10 pin 2 of the LPCXpresso board.&lt;/P&gt;
&lt;P&gt;I suggest you to use this video for reference: &lt;A href="https://www.nxp.com/document/guide/get-started-with-the-om13094:NGS-OM13094" target="_blank"&gt;https://www.nxp.com/document/guide/get-started-with-the-om13094:NGS-OM13094&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 21:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1290927#M45419</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-06-10T21:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1290954#M45421</link>
      <description>&lt;P&gt;Hello Omar,&lt;/P&gt;&lt;P&gt;yes I removed the resistor from the cable and already watched the video (Saw in schematic 120ohm already on Board). I followed every step in the video and also did a debugsession through the Loopback programm. All jumpers are connected.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks you for your help,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nils&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 23:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1290954#M45421</guid>
      <dc:creator>Neolinga</dc:creator>
      <dc:date>2021-06-10T23:26:24Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1292144#M45464</link>
      <description>&lt;P&gt;Hello Nils&lt;/P&gt;
&lt;P&gt;I replicated the example with wires since I don’t have db9 connectors. First I closed the jumpers to have a termination and wired the CANH and CANL. This worked well on my side, I suggest you replicate this with wires.&lt;BR /&gt;Your Db9 cable might not work as expected.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Omar_Anguiano_2-1623711357405.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/147052iCD22C93D71A925A0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Omar_Anguiano_2-1623711357405.jpeg" alt="Omar_Anguiano_2-1623711357405.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Omar_Anguiano_2-1623711357405.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 22:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1292144#M45464</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-06-14T22:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1295007#M45541</link>
      <description>&lt;P&gt;Hello Omar,&lt;/P&gt;&lt;P&gt;thank you alot for your patience &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt; I am glad to have such a good community here.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I connected the board to another USB port and it works now... seems the USB HUB is facing some problems. But anyway the example runs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I connected CANoe to analyze the message in parallel and wanted to enter a static message from our DBC. I managed to find the configure values for the data rate, ID and DLC. But i dont know how to enter the Data values. In the DBC and CANoe i have the raw data values in this format (DLC=32)&lt;/P&gt;&lt;P&gt;{ 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x01, 0xFF, 0x01, 0xFF, 0x00, 0x00, 0x00, 0x04, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 };&lt;/P&gt;&lt;P&gt;Where can i enter this value for the message and in which format it has to be?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you again for your patience...&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question - is there a way to pay for online support (of course with paying) or is the community forum the "only" way to get help here? I mean I want to give something back if you are supporting me.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nils&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Jun 2021 11:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1295007#M45541</guid>
      <dc:creator>Neolinga</dc:creator>
      <dc:date>2021-06-20T11:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: CAN-FD Simultation with LPCXpresso54628 and OM13099</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1565333#M50952</link>
      <description>&lt;P&gt;I have doubts about the implementation of CAN with two LPCXpresso54628 boards. If someone could help me I will attach the post below.&lt;/P&gt;&lt;P&gt;&lt;A title="NXP Forum" href="https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54628-Two-boards-CAN-Communication-MCUXpresso/m-p/1559586" target="_self"&gt;Forum: LPCXpresso54628-Two-boards-CAN-Communication-MCUXpresso&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 17:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-FD-Simultation-with-LPCXpresso54628-and-OM13099/m-p/1565333#M50952</guid>
      <dc:creator>Sam_B</dc:creator>
      <dc:date>2022-12-06T17:04:23Z</dc:date>
    </item>
  </channel>
</rss>