<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC54018 USB In-System Programming</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1286215#M45263</link>
    <description>&lt;P&gt;You should read on chapter 3 (non secure) and 4 (secure) based on your specific need.&lt;/P&gt;&lt;P&gt;Based on ISP / OTP bits, NXP boot allows you to download and launch a firmware&amp;nbsp; from USB into RAM. If you want to program internal flash then you need to write a firmware to do or you can re-use mcu-boot (part of the SDK) to do so. i.e. :&lt;/P&gt;&lt;P&gt;1) ISP download MCU-boot from USB to RAM&lt;/P&gt;&lt;P&gt;2)use blhost.exe to interact with MCU-boot to actually program your custom firmware into flash.&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jun 2021 15:41:01 GMT</pubDate>
    <dc:creator>belmontbob59</dc:creator>
    <dc:date>2021-06-02T15:41:01Z</dc:date>
    <item>
      <title>LPC54018 USB In-System Programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1286026#M45253</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Anyone has experienced with usb isp mode using LP54018?&lt;/P&gt;&lt;P&gt;Is there any document/sample project that I can refer to other than the user manual?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 09:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1286026#M45253</guid>
      <dc:creator>mohd_</dc:creator>
      <dc:date>2021-06-02T09:29:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 USB In-System Programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1286215#M45263</link>
      <description>&lt;P&gt;You should read on chapter 3 (non secure) and 4 (secure) based on your specific need.&lt;/P&gt;&lt;P&gt;Based on ISP / OTP bits, NXP boot allows you to download and launch a firmware&amp;nbsp; from USB into RAM. If you want to program internal flash then you need to write a firmware to do or you can re-use mcu-boot (part of the SDK) to do so. i.e. :&lt;/P&gt;&lt;P&gt;1) ISP download MCU-boot from USB to RAM&lt;/P&gt;&lt;P&gt;2)use blhost.exe to interact with MCU-boot to actually program your custom firmware into flash.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 15:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1286215#M45263</guid>
      <dc:creator>belmontbob59</dc:creator>
      <dc:date>2021-06-02T15:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 USB In-System Programming</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1294331#M45525</link>
      <description>&lt;P&gt;////&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jun 2021 23:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54018-USB-In-System-Programming/m-p/1294331#M45525</guid>
      <dc:creator>mohd_</dc:creator>
      <dc:date>2021-06-21T23:51:02Z</dc:date>
    </item>
  </channel>
</rss>