<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55xx GPIO in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1284332#M45222</link>
    <description>&lt;P&gt;Hello ianbenton,&lt;/P&gt;
&lt;P&gt;The maximum current trough the protection diodes is not characterized in the datasheet. There are some pin static characteristics including input current which would be the recommended limit.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
    <pubDate>Fri, 28 May 2021 23:26:15 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2021-05-28T23:26:15Z</dc:date>
    <item>
      <title>LPC55xx GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1282528#M45157</link>
      <description>&lt;P&gt;Are the GPIO inputs 5V tolerant?&lt;BR /&gt;If not, are there protection diodes from input to Vdd and Vss, so that it would be possible to connect a 5V input simply by using a current limiting resistor and allowing the upper protection diode to conduct (as is normally done in logic gates)?&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 11:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1282528#M45157</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-05-26T11:13:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1283692#M45185</link>
      <description>&lt;P&gt;Hello ianbenton,&lt;/P&gt;
&lt;P&gt;The LPC55XX GPIOs are not 5V tolerant. Only the VBUS pin is 5V tolerant. For more details please refer to the LPC55XX Datasheet.&lt;/P&gt;
&lt;P&gt;My apologies for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 20:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1283692#M45185</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-05-27T20:10:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1283693#M45186</link>
      <description>&lt;P&gt;Not inconvenient if I find out now.&lt;/P&gt;&lt;P&gt;Only inconvenient if I find out AFTER I've made my pcb.&lt;/P&gt;&lt;P&gt;I don't see any spec for the maximum current through the protection diode.&lt;/P&gt;&lt;P&gt;Also, the spec implies that the maximum voltage on a GPIO pin is 3.6V regardless of the value of Vdd. i.e&amp;nbsp; the pin could be taken 1.8V above Vdd if Vdd were 1.8V.&lt;/P&gt;&lt;P&gt;Is this correct?&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 20:17:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1283693#M45186</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-05-27T20:17:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1283698#M45188</link>
      <description>&lt;P&gt;Found the maximum voltage spec elsewhere in the datasheet, but not the maximum current through the protection diodes.&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 20:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1283698#M45188</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-05-27T20:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55xx GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1284332#M45222</link>
      <description>&lt;P&gt;Hello ianbenton,&lt;/P&gt;
&lt;P&gt;The maximum current trough the protection diodes is not characterized in the datasheet. There are some pin static characteristics including input current which would be the recommended limit.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 23:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55xx-GPIO/m-p/1284332#M45222</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-05-28T23:26:15Z</dc:date>
    </item>
  </channel>
</rss>