<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: What does locking the CFPA actually mean?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1284281#M45219</link>
    <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;-&amp;gt;&amp;gt; Yes, you can't program lash never.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;If it is never safe to lock the CFPA as I loose access to revoke etc. then why on earth is locking it possible? Things are tricky enough in this area without providing an extra way to shoot yourself in the foot.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;</description>
    <pubDate>Fri, 28 May 2021 20:29:08 GMT</pubDate>
    <dc:creator>andrewfisher</dc:creator>
    <dc:date>2021-05-28T20:29:08Z</dc:date>
    <item>
      <title>What does locking the CFPA actually mean?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1280492#M45093</link>
      <description>&lt;P&gt;I am using an LPC55S28 device and am trying to enable secure boot without shooting myself in the foot and bricking the device.&lt;/P&gt;&lt;P&gt;The UM11126 user guide explains that the CMPA and CFPA can be locked by writing the SH256 hash at the end. If I understand this correctly this means that I can program the CMPA and CFPA repeatedly if I do not update this hash. Is that correct?&lt;/P&gt;&lt;P&gt;Is this also true for the monotonic fields too? Can they be reset freely if not locked?&lt;/P&gt;&lt;P&gt;With regards to the CFPA what does it actually mean to lock it. If I lock it then it seams that I can never again flash new firmware, signed or not, as the revocation fields etc will no longer be updatable. At very least I loose the ability to ever revoke keys etc. Am I missing something here?&lt;/P&gt;&lt;P&gt;Also where is the CFPA located the UM says 0x003DE00 but some docs and questions refer to it being at 0x009DE00&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 16:06:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1280492#M45093</guid>
      <dc:creator>andrewfisher</dc:creator>
      <dc:date>2021-05-21T16:06:27Z</dc:date>
    </item>
    <item>
      <title>Re: What does locking the CFPA actually mean?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1281065#M45106</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;andrewfisher,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The UM11126 user guide explains that the CMPA and CFPA can be locked by writing the SH256 hash at the end. If I understand this correctly this means that I can program the CMPA and CFPA repeatedly if I do not update this hash. Is that correct?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; No, it depends on&amp;nbsp;Lifecycle state, about detail please refer to:&lt;/P&gt;
&lt;P&gt;UM11126-&amp;gt;&amp;nbsp;10.3 LPC55S69 Customer Development Lifecycle state.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With regards to the CFPA what does it actually mean to lock it. If I lock it then it seams that I can never again flash new firmware, signed or not, as the revocation fields etc will no longer be updatable. At very least I loose the ability to ever revoke keys etc. Am I missing something here?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; Yes, you can't program lash never.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also where is the CFPA located the UM says 0x003DE00 but some docs and questions refer to it being at 0x009DE00&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt;&amp;nbsp;0x009DE00 is right.&amp;nbsp;0x003DE00 is typo, it the address for lpc55s1x.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BTW, for secure boot, please refer to&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN12283.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 10:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1281065#M45106</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-05-24T10:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: What does locking the CFPA actually mean?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1284281#M45219</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;-&amp;gt;&amp;gt; Yes, you can't program lash never.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;If it is never safe to lock the CFPA as I loose access to revoke etc. then why on earth is locking it possible? Things are tricky enough in this area without providing an extra way to shoot yourself in the foot.&lt;/P&gt;&lt;P&gt;What am I missing?&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 20:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-does-locking-the-CFPA-actually-mean/m-p/1284281#M45219</guid>
      <dc:creator>andrewfisher</dc:creator>
      <dc:date>2021-05-28T20:29:08Z</dc:date>
    </item>
  </channel>
</rss>