<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: CAN</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1283105#M45173</link>
    <description>&lt;P&gt;Check the CANbus specification, e.g. on Wikipedia. The signal is pseudo differential, with H/L (or 1/0) levels different from the digital signal of the MCU pins. Therefore you need a transceiver.&lt;/P&gt;&lt;P&gt;If you want to test CAN on board level (without a real CAN network), you can get away without a transceiver, if both nodes in close proximity.&lt;/P&gt;&lt;P&gt;Most CAN peripherals use this for a configurable loop-back mode, were the Tx signal is fed directly back to the Rx signal. Usually for test purposes.&lt;/P&gt;&lt;P&gt;Setting up a larger CAN network is not really trivial, I would suggest an experienced mentor if you want/need to do so.&lt;/P&gt;</description>
    <pubDate>Thu, 27 May 2021 06:09:31 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2021-05-27T06:09:31Z</dc:date>
    <item>
      <title>CAN</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282591#M45158</link>
      <description>&lt;P&gt;Hi all, I am using the LPC54616, and I need to use the CAN protocol, I have seen that there are two CAN lines, a TD transmission line and a RD reception line.&lt;BR /&gt;Do I need a transceiver?&lt;BR /&gt;&lt;BR /&gt;If so, would the MCP2551 work for me?&lt;/P&gt;&lt;P&gt;Thank you all very much. Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 13:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282591#M45158</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-05-26T13:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: CAN</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282612#M45159</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; Do I need a transceiver?&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;gt; If so, would the MCP2551 work for me?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Yes to both questions.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 14:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282612#M45159</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-05-26T14:09:57Z</dc:date>
    </item>
    <item>
      <title>Re: CAN</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282623#M45160</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137574"&gt;@frank_m&lt;/a&gt;&amp;nbsp;THANK YOU VERY MUCH!!!&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 14:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282623#M45160</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-05-26T14:26:52Z</dc:date>
    </item>
    <item>
      <title>Re: CAN</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282633#M45161</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137574"&gt;@frank_m&lt;/a&gt;&amp;nbsp;But then what are the CAN outputs of the microcontroller for? If the transceiver with one transmitter and one receiver is enough.&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 14:42:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1282633#M45161</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-05-26T14:42:29Z</dc:date>
    </item>
    <item>
      <title>Re: CAN</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1283105#M45173</link>
      <description>&lt;P&gt;Check the CANbus specification, e.g. on Wikipedia. The signal is pseudo differential, with H/L (or 1/0) levels different from the digital signal of the MCU pins. Therefore you need a transceiver.&lt;/P&gt;&lt;P&gt;If you want to test CAN on board level (without a real CAN network), you can get away without a transceiver, if both nodes in close proximity.&lt;/P&gt;&lt;P&gt;Most CAN peripherals use this for a configurable loop-back mode, were the Tx signal is fed directly back to the Rx signal. Usually for test purposes.&lt;/P&gt;&lt;P&gt;Setting up a larger CAN network is not really trivial, I would suggest an experienced mentor if you want/need to do so.&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 06:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN/m-p/1283105#M45173</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-05-27T06:09:31Z</dc:date>
    </item>
  </channel>
</rss>