<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Convert from LPC15xx to LPC55xx</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1282091#M45136</link>
    <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well.&lt;BR /&gt;The LPC15 is part of the product longevity program and it will be part of it until Feb 2024 while the LPC55xx will be at that program until 2034/2035: &lt;A href="https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM" target="_blank"&gt;https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM &lt;/A&gt;&lt;BR /&gt;To verify if it is a good choice we need your application requirements.&lt;/P&gt;
&lt;P&gt;The LPC55 does not have the SWM module.&lt;BR /&gt;The Timers can be similar, but the internal structure is different. &lt;BR /&gt;The CAN controller from the LPC15 and the LPC55 is different, I suggest you refer to this application note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12728.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12728.pdf&lt;/A&gt;&lt;BR /&gt;The CAN-FD is an extension of the CAN protocol so you can use the module of the LPC55xx.&lt;/P&gt;
&lt;P&gt;To get started I suggest you refer to the SDK examples: &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
    <pubDate>Wed, 26 May 2021 00:04:19 GMT</pubDate>
    <dc:creator>Omar_Anguiano</dc:creator>
    <dc:date>2021-05-26T00:04:19Z</dc:date>
    <item>
      <title>Convert from LPC15xx to LPC55xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1280349#M45088</link>
      <description>&lt;P&gt;It appears as though the LPC55xx is easier to obtain than the LPC15xx.&amp;nbsp; It also seems to be higher spec and cheaper.&amp;nbsp;Would it be advisable to convert to the LPC55? Will the LPC15 eventually be phased out in favour of the LPC55? Or is there a better one to use?&lt;/P&gt;&lt;P&gt;A few queries in converting:&lt;/P&gt;&lt;P&gt;Does the LPC55 have a SWM peripheral?&lt;BR /&gt;The LPC55 has 1 of the SCT timers and several timers similar to those in the LPC11. Is that correct?&lt;/P&gt;&lt;P&gt;How do I convert the CAN software? I don't need CAN-FD. Is there an application note comparing the two different CAN peripherals.&lt;/P&gt;&lt;P&gt;What does the LPC55 need to get it started? On the LPC11/13/15 I have to enable the crystal oscillator and then change over when the oscillator has started. Is the LPC55 the same?&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 10:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1280349#M45088</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-05-21T10:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: Convert from LPC15xx to LPC55xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1282091#M45136</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Hope you are well.&lt;BR /&gt;The LPC15 is part of the product longevity program and it will be part of it until Feb 2024 while the LPC55xx will be at that program until 2034/2035: &lt;A href="https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM" target="_blank"&gt;https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM &lt;/A&gt;&lt;BR /&gt;To verify if it is a good choice we need your application requirements.&lt;/P&gt;
&lt;P&gt;The LPC55 does not have the SWM module.&lt;BR /&gt;The Timers can be similar, but the internal structure is different. &lt;BR /&gt;The CAN controller from the LPC15 and the LPC55 is different, I suggest you refer to this application note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12728.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12728.pdf&lt;/A&gt;&lt;BR /&gt;The CAN-FD is an extension of the CAN protocol so you can use the module of the LPC55xx.&lt;/P&gt;
&lt;P&gt;To get started I suggest you refer to the SDK examples: &lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 00:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1282091#M45136</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-05-26T00:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: Convert from LPC15xx to LPC55xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1282385#M45151</link>
      <description>&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;The facilities I use on the LPC15xx are A/D, comparator, timers, flash API, UART, CAN, I2C and SPI.&lt;/P&gt;&lt;P&gt;It is nice to have 16 bit A/Ds, but being restricted to just 7 inputs is a little disappointing. Some applications are going to need an external A/D, but a cheap 8-bit device will do.&lt;/P&gt;&lt;P&gt;I don't see another device in your portfolio as suitable, unless I choose one with over 100 pins, which I would like to avoid as I occasionally have to replace one by hand.&lt;/P&gt;&lt;P&gt;M-CAN is no more or no less arcane than C-CAN - just different!&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 08:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Convert-from-LPC15xx-to-LPC55xx/m-p/1282385#M45151</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2021-05-26T08:08:56Z</dc:date>
    </item>
  </channel>
</rss>