<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC11E1X Transistor size?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1281970#M45132</link>
    <description>&lt;P&gt;This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 May 2021 16:34:43 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2021-05-25T16:34:43Z</dc:date>
    <item>
      <title>LPC11E1X Transistor size?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1281883#M45129</link>
      <description>&lt;P&gt;I'm using the LPC11E14 in a project and I was just wondering what the transistor process size of this microcontroller is? Is it documented somewhere?&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 13:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1281883#M45129</guid>
      <dc:creator>haydenw</dc:creator>
      <dc:date>2021-05-25T13:49:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11E1X Transistor size?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1281970#M45132</link>
      <description>&lt;P&gt;This is not normally something that is publicised. However, I seem to remember that LPC11 is based on 130nm process (LPC18/43 is 90nm). The limiting factor for microcontrollers is flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 16:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1281970#M45132</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-05-25T16:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11E1X Transistor size?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1282469#M45156</link>
      <description>&lt;P&gt;Yeah okay it seems like I would have to contact NXP directly to get that information, thanks anyway for your insight.&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 09:39:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11E1X-Transistor-size/m-p/1282469#M45156</guid>
      <dc:creator>haydenw</dc:creator>
      <dc:date>2021-05-26T09:39:47Z</dc:date>
    </item>
  </channel>
</rss>