<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC5528 USB1_VBUS 5V tolerant? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1278920#M45066</link>
    <description>&lt;P&gt;"&lt;SPAN&gt;If the USB_VBUS function is connected to the USB connector and the device is self-powered, the USB_VBUS pin must be protected for situations when VDD = 0 V."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is exactly&amp;nbsp;the case. A self powered&amp;nbsp;device and it gets really&amp;nbsp;hot when VDD=0 and USB_VBUS is present.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 19 May 2021 10:36:02 GMT</pubDate>
    <dc:creator>microcris</dc:creator>
    <dc:date>2021-05-19T10:36:02Z</dc:date>
    <item>
      <title>LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1239537#M44125</link>
      <description>&lt;P&gt;Hello &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;LPC5528 datasheet states that this pin (pin 25 for&amp;nbsp;LPC5528JBD64K) is 5V tolerant, but if I connect it directly to 5V, the&amp;nbsp;LPC5528 gets really really hot and the USB connection gets lost.&amp;nbsp;&lt;BR /&gt;If I put a voltage divider in the&amp;nbsp;USB1_VBUS, the connection is stable and there is no heat in the&amp;nbsp;LPC5528.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was connecting it like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="microcris_1-1614793665774.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138637iC37A3F40CE16D02E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="microcris_1-1614793665774.png" alt="microcris_1-1614793665774.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;microcris_1-1614793665774.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="microcris_3-1614793730519.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138639iE465159D54A9FDE9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="microcris_3-1614793730519.png" alt="microcris_3-1614793730519.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;microcris_3-1614793730519.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, is it really 5V tolerant?&lt;/P&gt;&lt;P&gt;Thank you for seeing this &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 17:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1239537#M44125</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2021-03-03T17:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1240522#M44150</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;The pin is 5V tolerant only when VDD is applied at operating voltage level. I suggest you check the current of the pin, that current may be the cause of this heating. &lt;BR /&gt;&lt;BR /&gt;Let me know if this is helpful, if you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 21:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1240522#M44150</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-03-04T21:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1240767#M44155</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; The pin is 5V tolerant only when VDD is applied at operating voltage level.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am not sure if that is clear enough.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;All operation conditions (like voltage) apply only in a powered state, i.e. VDD applied. In power-off state, any voltage on other pins beyond (usually) 0.3V will be harmful.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 06:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1240767#M44155</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-03-05T06:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1240979#M44163</link>
      <description>&lt;P&gt;It took me a little bit to get there but eventually I understood that&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/169053"&gt;@Omar_Anguiano&lt;/a&gt;&amp;nbsp;&amp;nbsp;was saying the device needs to be fully operational (fully power supplied) in order to get the 5V tolerance in the mentioned pin.&lt;/P&gt;&lt;P&gt;I case the MCU power supply is not coming from the USB port (which is my case), I understand now that it is not possible to have a direct connection between the USB connector 5V pin and the&amp;nbsp;USB1_VBUS pin without power supplying&amp;nbsp;the entire MCU. I suppose that a 10kOhm resistor between those 2 pins will solve&amp;nbsp;the problem.&lt;/P&gt;&lt;P&gt;Regarding the situation where the MCU is fully power supplied, I ordered more LPC5528 microcontrollers and I cannot confirm anything else until I receive them...&lt;BR /&gt;...BUT I'm almost certain that I had the device power supplied, I was seeing the&amp;nbsp;"dmesg -w" output in the linux terminal and I was checking the mcu temperature with my finger. At some point the MCU got really hot and the USB connection got lost.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 12:19:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1240979#M44163</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2021-03-05T12:19:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1242727#M44203</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;If the USB_VBUS function is connected to the USB connector and the device is self-powered, the USB_VBUS pin must be protected for situations when VDD = 0 V. &lt;BR /&gt;If this is not the case with your application then I suggest you check the current supplied to the VBUS, a current that exceeds the ratings may be the cause of this heating.&lt;/P&gt;
&lt;P&gt;If you have more questions do not hesitate to ask me.&lt;BR /&gt;Best regards,&lt;BR /&gt;Omar&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 19:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1242727#M44203</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2021-03-09T19:28:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1278920#M45066</link>
      <description>&lt;P&gt;"&lt;SPAN&gt;If the USB_VBUS function is connected to the USB connector and the device is self-powered, the USB_VBUS pin must be protected for situations when VDD = 0 V."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is exactly&amp;nbsp;the case. A self powered&amp;nbsp;device and it gets really&amp;nbsp;hot when VDD=0 and USB_VBUS is present.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 10:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1278920#M45066</guid>
      <dc:creator>microcris</dc:creator>
      <dc:date>2021-05-19T10:36:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5528 USB1_VBUS 5V tolerant?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1486882#M49531</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm currently looking into the product data sheet of LPC55S2x/LPC552x which should also cover the LPC5528.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding pin 25 (USB1_VBUS), the data sheet refers to footnote [8] which states:&lt;/P&gt;&lt;P&gt;"The corresponding VBUS must be connected to supply voltage when using the USB peripheral. USB0_VBUS &lt;STRONG&gt;is not 5 V tolerant&lt;/STRONG&gt; pin. "&lt;/P&gt;&lt;P&gt;I'm puzzled. This seems contradictory to what is stated in this thread.&lt;/P&gt;&lt;P&gt;Is this pin 5 V tolerant and more generally, are the other digital input pins 5V tolerant?&lt;/P&gt;&lt;P&gt;I assume not as the data sheet on page 73 shows that Vi maximums is VDD + 0.5 V.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielholala_0-1657289750672.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186091iEE4A986F9B75AFE4/image-size/large?v=v2&amp;amp;px=999" role="button" title="danielholala_0-1657289750672.png" alt="danielholala_0-1657289750672.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielholala_0-1657289750672.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please advise.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 14:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5528-USB1-VBUS-5V-tolerant/m-p/1486882#M49531</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2022-07-08T14:16:01Z</dc:date>
    </item>
  </channel>
</rss>