<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Locking Sections of the LPC55S2x Flash in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278849#M45057</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;What choices do I have regarding preventing change to my software?&lt;/P&gt;&lt;P&gt;Can I then use the IAP FFR Driver through the CMPA configuration to enforce a signature check and SHA256 validation on the image on boot?&lt;BR /&gt;What happens if this check fails?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sachin Patel&lt;/P&gt;</description>
    <pubDate>Wed, 19 May 2021 09:23:49 GMT</pubDate>
    <dc:creator>sachin_patel</dc:creator>
    <dc:date>2021-05-19T09:23:49Z</dc:date>
    <item>
      <title>Locking Sections of the LPC55S2x Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278717#M45051</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to lock specific sections of the LPC55S2x flash (the user data region)? If the flash can be locked, can it be unlocked from within the locked portion of flash?&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Sachin Patel&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 07:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278717#M45051</guid>
      <dc:creator>sachin_patel</dc:creator>
      <dc:date>2021-05-19T07:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: Locking Sections of the LPC55S2x Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278825#M45056</link>
      <description>&lt;P&gt;Hi, Sachia,&lt;/P&gt;
&lt;P&gt;As far as I know that the LPC55S2x does not support the feature to lock a page, or section.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 09:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278825#M45056</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-05-19T09:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: Locking Sections of the LPC55S2x Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278849#M45057</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your response.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;What choices do I have regarding preventing change to my software?&lt;/P&gt;&lt;P&gt;Can I then use the IAP FFR Driver through the CMPA configuration to enforce a signature check and SHA256 validation on the image on boot?&lt;BR /&gt;What happens if this check fails?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sachin Patel&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 09:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278849#M45057</guid>
      <dc:creator>sachin_patel</dc:creator>
      <dc:date>2021-05-19T09:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: Locking Sections of the LPC55S2x Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278877#M45060</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Pls refer to the an13037.pdf from the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13037.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN13037.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It talks about how to block SWD and protect customer code in flash.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 09:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1278877#M45060</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-05-19T09:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: Locking Sections of the LPC55S2x Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1280469#M45092</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is not what I am asking about.&lt;/P&gt;&lt;P&gt;Is there a way to ensure that the flash remains unchanged during operation, such as a flash write protect?&lt;/P&gt;&lt;P&gt;Secure Boot is an option, but it does not ensure the image is not altered at runtime, only on startup, which isn’t quite what I am looking for.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sachin Patel&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 14:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1280469#M45092</guid>
      <dc:creator>sachin_patel</dc:creator>
      <dc:date>2021-05-21T14:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: Locking Sections of the LPC55S2x Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1281749#M45123</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, there is not a mechanism to protect flash from erasing/programming.&lt;/P&gt;
&lt;P&gt;Pls refer to the Chapter&amp;nbsp; 5: LPC55S6x/LPC55S2x/LPC552x Flash in UM11126.pdf.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Tue, 25 May 2021 10:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Locking-Sections-of-the-LPC55S2x-Flash/m-p/1281749#M45123</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-05-25T10:12:03Z</dc:date>
    </item>
  </channel>
</rss>