<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: I receive the correct temperature from one LM35, while receive a constant number from the other</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1277097#M45013</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp; What do you think about this? Last time you helped me with this code and it worked&lt;/P&gt;</description>
    <pubDate>Fri, 14 May 2021 18:30:05 GMT</pubDate>
    <dc:creator>Alex_2221</dc:creator>
    <dc:date>2021-05-14T18:30:05Z</dc:date>
    <item>
      <title>I receive the correct temperature from one LM35, while receive a constant number from the other one</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1276568#M45004</link>
      <description>&lt;P&gt;Hello everyone, I'm using adcs of LPC1768 to read 2 temperatures of two LM35 sensors. I receive the correct temperature from one of the sensors, but keep receiving a constant number like 151 from the other one. My code used to work fine before, but I had to reprogram my board with another computer and all of a sudden this problem showed up. I added the C files of keil. I was wondering if you you'd mind helping me resolve this issue&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 19:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1276568#M45004</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-05-13T19:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: I receive the correct temperature from one LM35, while receive a constant number from the other</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1277097#M45013</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp; What do you think about this? Last time you helped me with this code and it worked&lt;/P&gt;</description>
      <pubDate>Fri, 14 May 2021 18:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1277097#M45013</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-05-14T18:30:05Z</dc:date>
    </item>
    <item>
      <title>Re: I receive the correct temperature from one LM35, while receive a constant number from the other</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1277727#M45028</link>
      <description>&lt;P&gt;Hi Alex,&lt;/P&gt;
&lt;P&gt;If there was no modification to the code then software should not be an issue. I would check hardware connections, if sensor is appropriately connected or even testing with an external power supply instead of sensor.&lt;/P&gt;
&lt;P&gt;If you think code maybe was modified then I recommend you to compare register configuration for each channel and see if there is any difference.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 17:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1277727#M45028</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-05-17T17:01:24Z</dc:date>
    </item>
    <item>
      <title>Re: I receive the correct temperature from one LM35, while receive a constant number from the other</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1278098#M45033</link>
      <description>&lt;P&gt;Thanks for the reply, yeah there was a hardware issue and I resolved it. Thank you so much&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 08:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-receive-the-correct-temperature-from-one-LM35-while-receive-a/m-p/1278098#M45033</guid>
      <dc:creator>Alex_2221</dc:creator>
      <dc:date>2021-05-18T08:46:23Z</dc:date>
    </item>
  </channel>
</rss>