<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RTC calibration in LPC55S69 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/RTC-calibration-in-LPC55S69/m-p/1276697#M45006</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;gnichimohamed,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry LPC55s69 doesn't support RTC calibration.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power&lt;BR /&gt;domain. A timer in the RTC can be used for wake-up from all low power modes&lt;BR /&gt;including deep power-down, with 1 ms resolution. The RTC is clocked by the&lt;BR /&gt;32 kHz FRO or 32.768 kHz external crystal.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Fri, 14 May 2021 02:32:17 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2021-05-14T02:32:17Z</dc:date>
    <item>
      <title>RTC calibration in LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/RTC-calibration-in-LPC55S69/m-p/1276470#M45002</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In the LPC55S69 there is no mentioning of RTC calibration, do you have any idea how we can do it?&lt;/P&gt;&lt;P&gt;Thanks for the help!&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 15:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/RTC-calibration-in-LPC55S69/m-p/1276470#M45002</guid>
      <dc:creator>gnichimohamed</dc:creator>
      <dc:date>2021-05-13T15:29:22Z</dc:date>
    </item>
    <item>
      <title>Re: RTC calibration in LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/RTC-calibration-in-LPC55S69/m-p/1276697#M45006</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;gnichimohamed,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry LPC55s69 doesn't support RTC calibration.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power&lt;BR /&gt;domain. A timer in the RTC can be used for wake-up from all low power modes&lt;BR /&gt;including deep power-down, with 1 ms resolution. The RTC is clocked by the&lt;BR /&gt;32 kHz FRO or 32.768 kHz external crystal.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 14 May 2021 02:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/RTC-calibration-in-LPC55S69/m-p/1276697#M45006</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-05-14T02:32:17Z</dc:date>
    </item>
  </channel>
</rss>