<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックDAC to LPC54616</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-to-LPC54616/m-p/1276250#M44996</link>
    <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I was wondering if someone could recommend a DAC for use with the LPC54616 microcontroller, which is powered at 3.3V.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The aim is to convert a PWM signal generated by the microcontroller into a triangular signal.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 13 May 2021 07:56:54 GMT</pubDate>
    <dc:creator>Nadia</dc:creator>
    <dc:date>2021-05-13T07:56:54Z</dc:date>
    <item>
      <title>DAC to LPC54616</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-to-LPC54616/m-p/1276250#M44996</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I was wondering if someone could recommend a DAC for use with the LPC54616 microcontroller, which is powered at 3.3V.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The aim is to convert a PWM signal generated by the microcontroller into a triangular signal.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 07:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-to-LPC54616/m-p/1276250#M44996</guid>
      <dc:creator>Nadia</dc:creator>
      <dc:date>2021-05-13T07:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: DAC to LPC54616</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-to-LPC54616/m-p/1277312#M45018</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;NXP has&amp;nbsp;8-bit I2C A/D and D/A converter PCF8591. Operating supply voltage 2.5 V to 6.0 V&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/interfaces/ic-spi-serial-interface-devices/ic-dacs-and-adcs/8-bit-a-d-and-d-a-converter:PCF8591" target="_blank" rel="noopener"&gt;https://www.nxp.com/products/interfaces/ic-spi-serial-interface-devices/ic-dacs-and-adcs/8-bit-a-d-and-d-a-converter:PCF8591&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For more DAC, I suggest you checking 3rd parties, for example ADI.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 17 May 2021 03:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DAC-to-LPC54616/m-p/1277312#M45018</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-05-17T03:03:12Z</dc:date>
    </item>
  </channel>
</rss>