<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC54114: what's the maximum CPU speed? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1270844#M44864</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to confirm that importing CLOCK_SetupFROClocking() and POWER_SetVoltageForFreq() from SDK 2.9.0 to mcuxpresso_v3.01.000 libraries seems to have solved the problem and now I can setup clock speed up to 150MHz.&lt;/P&gt;&lt;P&gt;So, the bug seems to be restricted to libpower library into functions Chip_POWER_SetVoltage() and Chip_POWER_SetFROHFRate().&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;</description>
    <pubDate>Fri, 30 Apr 2021 12:44:17 GMT</pubDate>
    <dc:creator>carlobramini</dc:creator>
    <dc:date>2021-04-30T12:44:17Z</dc:date>
    <item>
      <title>LPC54114: what's the maximum CPU speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1265705#M44727</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I'm using an OM13089 LPCXpresso5411x and I would like to push the CPUs to their maximum speed.&lt;BR /&gt;Unfortunately, I'm a bit confuse because:&lt;BR /&gt;1) the datasheet "Rev. 2.6 - 3 September 2020" says that the maximum speed is 150MHz.&lt;BR /&gt;2) The user's manual UM10914 "Rev. 2.0 - 9 May 2018" says that the maximum speed is 100MHz.&lt;BR /&gt;3) if I try to set something faster than 120MHz with mcuxpresso_v3.01.000 libraries, the M4 goes in Hardware Fault exception.&lt;/P&gt;&lt;P&gt;What's the real maximum speed and how to set it?&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 08:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1265705#M44727</guid>
      <dc:creator>carlobramini</dc:creator>
      <dc:date>2021-04-21T08:25:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54114: what's the maximum CPU speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1265712#M44728</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; 1) the datasheet "Rev. 2.6 - 3 September 2020" says that the maximum speed is 150MHz.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&amp;gt; 2) The user's manual UM10914 "Rev. 2.0 - 9 May 2018" says that the maximum speed is 100MHz.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The MCU version might have changed in the meantime, perhaps check the schematics.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt; if I try to set something faster than 120MHz with mcuxpresso_v3.01.000 libraries, the M4 goes in Hardware Fault exception.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Flash interface settings are tightly related to core speed.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;The higher the core clock, the more wait states you will need for the slower Flash. Too tight setting will lead to crashes and hardfaults.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;You might need to check the MCU user manual, and change your SDK example accordingly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I rarely mess with the core clock settings, haven't done it myself on a LPC.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 08:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1265712#M44728</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-04-21T08:35:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54114: what's the maximum CPU speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1266545#M44741</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;carlobramini,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;How about use MCUXpresso config tool configure clock , then just test a hello world demo ?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 09:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1266545#M44741</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-04-22T09:29:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54114: what's the maximum CPU speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1270254#M44852</link>
      <description>&lt;P&gt;Hello, thank you very much for the replies.&lt;/P&gt;&lt;P&gt;I tried to use MCUXpresso config tool and I have set 150MHz: I think it is working fine, although the CYCCNT register of DWT is not counting at that rate but MUCH slower. Then, I compared the sources of mcuxpresso_v3.01.000 libraries with the SDK_2.8.2_LPCXpresso54114 and I adjusted the function for setting the wait states of the flash, which was wrong according to the datasheet. Unfortunately, mcuxpresso_v3.01.000 libraries cannot still setup 150MHz... with the same parameters, it still goes to hardware fault. The only piece of code that I could not verify are differences between the function Chip_POWER_SetVoltage and POWER_SetVoltageForFreq, but unfortunately, there are not the sources for that. Since this is the only thing that I could not verify, I suspect that the bug could be there, if that function could not set up for 150MHz. Before giving up, I will try to import libpower.a from SDK to LPCOpen, to see if it will work.&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 09:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1270254#M44852</guid>
      <dc:creator>carlobramini</dc:creator>
      <dc:date>2021-04-29T09:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54114: what's the maximum CPU speed?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1270844#M44864</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to confirm that importing CLOCK_SetupFROClocking() and POWER_SetVoltageForFreq() from SDK 2.9.0 to mcuxpresso_v3.01.000 libraries seems to have solved the problem and now I can setup clock speed up to 150MHz.&lt;/P&gt;&lt;P&gt;So, the bug seems to be restricted to libpower library into functions Chip_POWER_SetVoltage() and Chip_POWER_SetFROHFRate().&lt;/P&gt;&lt;P&gt;Sincerely.&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 12:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54114-what-s-the-maximum-CPU-speed/m-p/1270844#M44864</guid>
      <dc:creator>carlobramini</dc:creator>
      <dc:date>2021-04-30T12:44:17Z</dc:date>
    </item>
  </channel>
</rss>