<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックBooting via SD Card</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-via-SD-Card/m-p/1270232#M44849</link>
    <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;Actually i am trying to boot the LPC55S69 board through SD Card, i am not sure how much it is feasible.&lt;/P&gt;&lt;P&gt;If yes, any docs and pointer is really help me to move forward.&lt;/P&gt;&lt;P&gt;Actually i am exploring ways to boot the Board other than MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;Another ways to boot is via a cmd line using &lt;STRONG&gt;JLinkGDBServer &lt;/STRONG&gt;in that also one need to use external debugger to flash&amp;nbsp; the program on to the&amp;nbsp; board.&lt;/P&gt;&lt;P&gt;Is there a way to flash the application using internal debugger without the use of external hardware.&lt;/P&gt;&lt;P&gt;Any help is really appreciated!&lt;/P&gt;</description>
    <pubDate>Thu, 29 Apr 2021 09:04:55 GMT</pubDate>
    <dc:creator>suvhm</dc:creator>
    <dc:date>2021-04-29T09:04:55Z</dc:date>
    <item>
      <title>Booting via SD Card</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-via-SD-Card/m-p/1270232#M44849</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;Actually i am trying to boot the LPC55S69 board through SD Card, i am not sure how much it is feasible.&lt;/P&gt;&lt;P&gt;If yes, any docs and pointer is really help me to move forward.&lt;/P&gt;&lt;P&gt;Actually i am exploring ways to boot the Board other than MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;Another ways to boot is via a cmd line using &lt;STRONG&gt;JLinkGDBServer &lt;/STRONG&gt;in that also one need to use external debugger to flash&amp;nbsp; the program on to the&amp;nbsp; board.&lt;/P&gt;&lt;P&gt;Is there a way to flash the application using internal debugger without the use of external hardware.&lt;/P&gt;&lt;P&gt;Any help is really appreciated!&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 09:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-via-SD-Card/m-p/1270232#M44849</guid>
      <dc:creator>suvhm</dc:creator>
      <dc:date>2021-04-29T09:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: Booting via SD Card</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-via-SD-Card/m-p/1271433#M44878</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Booting from SD card is not possible with this MCU. You can check boot modes in table 169 and 170 of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11126" target="_blank"&gt;User Manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Additionally, you can use Flash Magic to communicate with LPC55S69 in ISP mode. Please check the link below for more details.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/lpc%40tkb/201/3/Flash%20Magic%20programming%20LPC.pdf" target="_blank"&gt;https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/lpc%40tkb/201/3/Flash%20Magic%20programming%20LPC.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 May 2021 20:39:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Booting-via-SD-Card/m-p/1271433#M44878</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-05-03T20:39:30Z</dc:date>
    </item>
  </channel>
</rss>