<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC2368 Watchdog triggered on heat in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269380#M44810</link>
    <description>&lt;P&gt;Many parameter depend on temperature, and timing gets worse with higher temperatures.&lt;/P&gt;&lt;P&gt;I think you watchdog triggers because Flash fetches fail. Your Flash setup (core clock speed, wait states) are approriate for normal temperatures, but most probably fail at higher temperature.&lt;/P&gt;&lt;P&gt;This would also explain the seemingly random location.&lt;/P&gt;&lt;P&gt;You could try more relaxed (i.e. more generous) wait state settings, or a reduced core clock. Alternatively, shut down the device at critical temperatures.&lt;/P&gt;&lt;P&gt;I remember a project I once worked on, that also failed at similar temperatures. While the MCU was still fine, all the optocoupler signals it heavily relied on had basically "disappeared".&lt;/P&gt;</description>
    <pubDate>Wed, 28 Apr 2021 06:18:38 GMT</pubDate>
    <dc:creator>frank_m</dc:creator>
    <dc:date>2021-04-28T06:18:38Z</dc:date>
    <item>
      <title>LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269289#M44804</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have a product using the LPC2368 for years now. The software/firmware has two parts: Boot code and Main code. Both stored in the same Internal Flash, but Main code is in upper address boundary. The Boot code can verify if the Main code is valid; and can jump to the Main code. Interface to this product is done via USB.&lt;/P&gt;&lt;P&gt;We have a &lt;STRONG&gt;few&lt;/STRONG&gt; boards wherein the &lt;STRONG&gt;Watchdog&lt;/STRONG&gt; is triggered when heat is applied to the board (65 to 80 celsius). The LPC2368 is rated to work for LPC2368.&lt;/P&gt;&lt;P&gt;We've been &lt;STRONG&gt;trying to track&amp;nbsp;&lt;/STRONG&gt;the point BEFORE the Watchdog is triggered. However, it seems to being triggered in &lt;STRONG&gt;several random places&lt;/STRONG&gt;. We're using one of the UARTs for debugging/tracing. On a few occasions when the Watchdog is triggered and the Boot code runs, it even reports that the Main code is &lt;STRONG&gt;INVALID or CORRUPTED.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Some questions:&lt;/P&gt;&lt;P&gt;1. Is there any other way (besides using UART tracing) to detect at what point did the software hanged up the Watchdog is triggered?&lt;/P&gt;&lt;P&gt;2. What are the other possible peripherals (XTAL, etc.), that can cause software hangup? As noted - it seems to random places.&lt;/P&gt;&lt;P&gt;3. How can the Boot code report that the Main code is &lt;STRONG&gt;INVALID or CORRUPTED&lt;/STRONG&gt;? Since both are sitting on the same Internal Flash.&lt;/P&gt;&lt;P&gt;Thanks for any feedback!&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 03:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269289#M44804</guid>
      <dc:creator>junointegration</dc:creator>
      <dc:date>2021-04-28T03:48:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269380#M44810</link>
      <description>&lt;P&gt;Many parameter depend on temperature, and timing gets worse with higher temperatures.&lt;/P&gt;&lt;P&gt;I think you watchdog triggers because Flash fetches fail. Your Flash setup (core clock speed, wait states) are approriate for normal temperatures, but most probably fail at higher temperature.&lt;/P&gt;&lt;P&gt;This would also explain the seemingly random location.&lt;/P&gt;&lt;P&gt;You could try more relaxed (i.e. more generous) wait state settings, or a reduced core clock. Alternatively, shut down the device at critical temperatures.&lt;/P&gt;&lt;P&gt;I remember a project I once worked on, that also failed at similar temperatures. While the MCU was still fine, all the optocoupler signals it heavily relied on had basically "disappeared".&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 06:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269380#M44810</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-04-28T06:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269543#M44819</link>
      <description>&lt;P&gt;Hi, Jun,&lt;/P&gt;
&lt;P&gt;I agree with Frank that the flash access may requires more delay cycles with temperature rising. pls change the MAMTIM with 7 and have try.&lt;/P&gt;
&lt;P&gt;With the temperature rising, you have not enough time delay when reading flash, the binary code your read is wrong, so the CPU will hang, the watchdog will function and reset the chip.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1619600733749.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/143517i9B28634BB7F525D9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1619600733749.png" alt="xiangjun_rong_0-1619600733749.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1619600733749.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 09:08:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269543#M44819</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-04-28T09:08:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269594#M44824</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, assuming you are in a kind of moderator role - the post from contributor "&lt;/SPAN&gt;&lt;SPAN&gt;jimiizx" in this thread here looks very suspiciously like spam, a.k.a. unsolicited advertisment.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please have a look at it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 10:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1269594#M44824</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-04-28T10:24:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1270077#M44838</link>
      <description>&lt;P&gt;I've actually disabled MAM for now and Watchdog has not been triggered so far (when applying heat to 75+ celsius)! Some bit of testing required on our side to understand the implications of this though.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some&amp;nbsp; additional questions:&lt;/P&gt;&lt;P&gt;1. The datasheet seems to indicate that MAM is disabled by default. But when the software runs after a reset, the CPU is indicating it is set to 2 (fully enabled). Does this mean that some initial batches of LPC2368 has it 0 (off), and newer batches has set it to 2 (fully enabled)?&lt;/P&gt;&lt;P&gt;2. We actually have another board which has the&amp;nbsp;Watchdog triggered intermittently even&amp;nbsp;&lt;STRONG&gt;without heat.&amp;nbsp;&lt;/STRONG&gt;Does this mean that there's an internal fault in the MAM of the CPU? Or is there a fault in the peripherals connected to the CPU?&lt;/P&gt;&lt;P&gt;3. Do you have a rough idea what is the performance penalty with MAM disabled? Will it be twice&amp;nbsp; slower than before?&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp; and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137574"&gt;@frank_m&lt;/a&gt;&amp;nbsp;again for response! Much appreciated!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 05:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1270077#M44838</guid>
      <dc:creator>junointegration</dc:creator>
      <dc:date>2021-04-29T05:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1270088#M44841</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; 3. Do you have a rough idea what is the performance penalty with MAM disabled? Will it be twice&amp;nbsp; slower than before?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;AFAIK (as a software guy), this is highly individual, i.e. might differ between instances of MCUs. This is why MCU vendors use to guarantee worst case conditions, and often list averages (Min/Typ/Max).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For a properly working product, you would need to expect the worst case ...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Cannot comment on the LPC2368, I never worked with that MCU.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 06:08:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1270088#M44841</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-04-29T06:08:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1270122#M44842</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Q1. The datasheet seems to indicate that MAM is disabled by default. But when the software runs after a reset, the CPU is indicating it is set to 2 (fully enabled). Does this mean that some initial batches of LPC2368 has it 0 (off), and newer batches has set it to 2 (fully enabled)?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;If the MAMTIM register is not the same with the default 0x07, I suppose it must be modified by the code somewhere.&lt;/P&gt;
&lt;P&gt;Q2. We actually have another board which has the&amp;nbsp;Watchdog triggered intermittently even&amp;nbsp;&lt;STRONG&gt;without heat.&amp;nbsp;&lt;/STRONG&gt;Does this mean that there's an internal fault in the MAM of the CPU? Or is there a fault in the peripherals connected to the CPU?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Yes, the MAMTIM value must match with your system clock frequency.&lt;/P&gt;
&lt;P&gt;7.9 MAM usage notes&lt;/P&gt;
&lt;P&gt;When changing MAM timing, the MAM must first be turned off by writing a zero to&lt;BR /&gt;MAMCR. A new value may then be written to MAMTIM. Finally, the MAM may be turned&lt;BR /&gt;on again by writing a value (1 or 2) corresponding to the desired operating mode to&lt;BR /&gt;MAMCR.&lt;BR /&gt;For a system clock slower than 20 MHz, MAMTIM can be 001. For a system clock&lt;BR /&gt;between 20 MHz and 40 MHz, flash access time is suggested to be 2 CCLKs, while in&lt;BR /&gt;systems with a system clock faster than 40 MHz, 3 CCLKs are proposed. For system&lt;BR /&gt;clocks of 60 MHz and above, 4CCLK’s are needed.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Q3. Do you have a rough idea what is the performance penalty with MAM disabled? Will it be twice&amp;nbsp; slower than before?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;If the MAM is disabled, I think the default 7 clcok cycles delay will be enabled. Regarding the performance penalty, I think reading flash will use 7 clock cycles delay, when the instruction is in the instruction pipeline, it will be fast.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Thu, 29 Apr 2021 07:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1270122#M44842</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-04-29T07:08:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2368 Watchdog triggered on heat</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1278521#M45044</link>
      <description>&lt;P&gt;We have been SOAK testing the suspected 'faulty' hardware now for weeks now. All was working OK with no Watchdog resets &lt;STRONG&gt;apart from one incident we saw yesterday &lt;/STRONG&gt;on one hardware.&lt;/P&gt;&lt;P&gt;Prior to disabling MAM, these suspected 'faulty' hardware were triggering Watchdog resets intermittently (one unit multiple times a day; some units once every 2-3 days).&amp;nbsp; It's likely that the latest Watchdog reset incident is due to the a faulty CPU or some other hardware fault - difficult to determine. The hardware has undergone several heat testing above 85 degrees celsius previously.&lt;/P&gt;&lt;P&gt;With regards to speed, disabling the MAM for the LPC2368 made it 3x slower. However, the actual application that we use does NOT seem to have any affect at all (as the application depend on timers ranging from 50ms to 1second). The LPC2368 is still fast with MAM disabled for our purpose.&lt;/P&gt;&lt;P&gt;I have revisited the LPC2368 errata sheet again. And did notice that MAM is mentioned in 3.12.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/errata/ES_LPC2364_66_68.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/errata/ES_LPC2364_66_68.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;However, the implications of the incorrect MAM setting is quite vague - does not mention about Watchdog resets or corruption of code.&lt;/P&gt;&lt;P&gt;Anyway, thanks again&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26034"&gt;@xiangjun_rong&lt;/a&gt;&amp;nbsp; and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137574"&gt;@frank_m&lt;/a&gt;&amp;nbsp; for your help!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 May 2021 01:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2368-Watchdog-triggered-on-heat/m-p/1278521#M45044</guid>
      <dc:creator>junointegration</dc:creator>
      <dc:date>2021-05-19T01:50:52Z</dc:date>
    </item>
  </channel>
</rss>