<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 dev board parodically requires hard reset to program it</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264639#M44708</link>
    <description>&lt;P&gt;Thanks for the help Converse. I am not sure if it an issue with the background process on the computer, I do not see &lt;SPAN&gt;redlinkserv in the process list in between flashing attempts. I also just noticed that the issue persists across a reset of the computer, in my mind that points towards&amp;nbsp;something go on with the dev board.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Apr 2021 00:29:32 GMT</pubDate>
    <dc:creator>plong44</dc:creator>
    <dc:date>2021-04-20T00:29:32Z</dc:date>
    <item>
      <title>LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264534#M44705</link>
      <description>&lt;P&gt;I have an LPCXpresso55S69 dev board hooked up to a Jenkins server and periodically the board gets into a state where it is not flashable with the command line (using crt_emu_cm_redlink).&lt;/P&gt;&lt;P&gt;crt_emu_cm_redlink reports the following error:&lt;/P&gt;&lt;P&gt;PS Z:\&amp;gt; &amp;amp; $MCUX_IDE_BIN/crt_emu_cm_redlink --flash-mass-load-exec "file.bin" -p LPC55S69 --load-base=0x0 --bootromstall 0x50000040 --flash-driver= -x C:/&amp;lt;Project Path&amp;gt;/Debug --flash-dir $MCUX_FLASH_DIR0 --flash-dir $MCUX_FLASH_DIR1 --flash-hashing&lt;BR /&gt;Ns: MCUXpresso IDE RedlinkMulti Driver v11.3 (Jan 11 2021 16:41:13 - crt_emu_cm_redlink.exe build 9)&lt;BR /&gt;Wc(03). No cache support.&lt;BR /&gt;Nc: Found chip XML file in C:/&amp;lt;Project Path&amp;gt;/Debug\LPC55S69.xml&lt;BR /&gt;Nc: Restarted LinkServer process (PID 11896).&lt;BR /&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;BR /&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;BR /&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;BR /&gt;Nc: Reconnected to existing LinkServer process.&lt;BR /&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;BR /&gt;Nc: Server OK but no connection to probe 0 core -2(ANY) (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;Ed:02: Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;Et:31: No connection to chip's debug port&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any hints or help resolving this issue would be much appreciated!&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 18:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264534#M44705</guid>
      <dc:creator>plong44</dc:creator>
      <dc:date>2021-04-19T18:11:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264538#M44706</link>
      <description>&lt;P&gt;Looks like the background process is having problems - make sure you kill the redlinkserv process before starting.&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 18:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264538#M44706</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-04-19T18:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264639#M44708</link>
      <description>&lt;P&gt;Thanks for the help Converse. I am not sure if it an issue with the background process on the computer, I do not see &lt;SPAN&gt;redlinkserv in the process list in between flashing attempts. I also just noticed that the issue persists across a reset of the computer, in my mind that points towards&amp;nbsp;something go on with the dev board.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 00:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1264639#M44708</guid>
      <dc:creator>plong44</dc:creator>
      <dc:date>2021-04-20T00:29:32Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1265693#M44725</link>
      <description>&lt;P&gt;How about test on another PC?&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 08:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1265693#M44725</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-04-21T08:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1265701#M44726</link>
      <description>&lt;P&gt;&lt;EM&gt;&amp;gt; I also just noticed that the issue persists across a reset of the computer, in my mind that points towards&amp;nbsp;something go on with the dev board.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I don't think so.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I suspect an issue with the configuration and/or setup. I suppose the redlink server is a separate process, communicating via socket interface. Which means, it could be susceptible to firewall / virus scanner software.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 08:19:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1265701#M44726</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-04-21T08:19:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1265989#M44734</link>
      <description>&lt;P&gt;That is an interesting point, I'll check the antivirus logs and whatnot for any evidence of interference. One thing that might not jive with your theory is that I am able to flash the board after I unplug it and plug it back in, if it was an antivirus/firewall issue I would think the problem would persist. Maybe that is a bad assumption though, thanks for help!&lt;/P&gt;</description>
      <pubDate>Wed, 21 Apr 2021 16:24:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1265989#M44734</guid>
      <dc:creator>plong44</dc:creator>
      <dc:date>2021-04-21T16:24:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1266445#M44739</link>
      <description>&lt;P&gt;Usually such issues often turn up with remote debug, were debugger and debug server run on different machines.&lt;/P&gt;&lt;P&gt;To be honest, I am not much into MCUxpresso debugger details, but just assume it is similar to GDB. Most Eclipse toolchains run a separate GDB server process on the same machine, comunicating via Unix domain sockets (dunno how you call that on Windows...).&lt;/P&gt;&lt;P&gt;Perhaps you can locate the config/init script for the debug server, and modify it for more verbose output. That might give you a clue.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Apr 2021 07:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1266445#M44739</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-04-22T07:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 dev board parodically requires hard reset to program it</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1269057#M44798</link>
      <description>&lt;P&gt;Thanks again for your help Frank. I ended up putting a relay (controlled by the PC) on the 5v line of a USB cable to allow me to programmatically reset the board. I'll probably try removing my relay board after the next mcuxpresso/windows/etc. update.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 16:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-dev-board-parodically-requires-hard-reset-to-program-it/m-p/1269057#M44798</guid>
      <dc:creator>plong44</dc:creator>
      <dc:date>2021-04-27T16:22:50Z</dc:date>
    </item>
  </channel>
</rss>