<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Sample LPCopen project  will not run/debug LPC11U68 board</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-LPCopen-project-will-not-run-debug-LPC11U68-board/m-p/1264393#M44700</link>
    <description>&lt;P&gt;I am able to compile the LPCopen examples but can not yet run or debug.&lt;/P&gt;&lt;P&gt;Using windows 10&amp;nbsp; connected to LPC11U68 board.&lt;/P&gt;&lt;P&gt;The redlink window reports:&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;/P&gt;&lt;P&gt;The example project is:&lt;/P&gt;&lt;P&gt;LPC11u6x Pin Interrupt example&lt;BR /&gt;===============================&lt;/P&gt;&lt;P&gt;Example description&lt;BR /&gt;-------------------&lt;BR /&gt;The Pin interrupt example demonstrates using the pin interrupt API functions&lt;BR /&gt;pin interrupts &amp;amp; wake up from low power sleep state using the pin&lt;BR /&gt;interrupts.&lt;/P&gt;&lt;P&gt;This example configures the pin interrupt channel 7 as falling edge&lt;BR /&gt;wake up interrupt. The interrupt channel 7 is connected to GPIO pin&lt;BR /&gt;PIO0-0 in GPIO block. The example will go to sleep mode. To wake up from&lt;BR /&gt;sleep mode, provide a falling edge pulse at GPIO pin PIO0-0.&lt;BR /&gt;On the LPCXpresso board, PIO0-0 is connected to pontentiometer which&lt;BR /&gt;can be used to provide falling edge pulse. The application will go to&lt;BR /&gt;sleep state in a loop, with every wake up the board LED0 will be toggled.&lt;/P&gt;&lt;P&gt;Special connection requirements&lt;BR /&gt;-------------------------------&lt;BR /&gt;The LPCXpresso base board is required with the LPCXpresso board to use this&lt;BR /&gt;example. The Manley board needs no extra hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 19 Apr 2021 13:51:25 GMT</pubDate>
    <dc:creator>jDrum</dc:creator>
    <dc:date>2021-04-19T13:51:25Z</dc:date>
    <item>
      <title>Sample LPCopen project  will not run/debug LPC11U68 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-LPCopen-project-will-not-run-debug-LPC11U68-board/m-p/1264393#M44700</link>
      <description>&lt;P&gt;I am able to compile the LPCopen examples but can not yet run or debug.&lt;/P&gt;&lt;P&gt;Using windows 10&amp;nbsp; connected to LPC11U68 board.&lt;/P&gt;&lt;P&gt;The redlink window reports:&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;/P&gt;&lt;P&gt;The example project is:&lt;/P&gt;&lt;P&gt;LPC11u6x Pin Interrupt example&lt;BR /&gt;===============================&lt;/P&gt;&lt;P&gt;Example description&lt;BR /&gt;-------------------&lt;BR /&gt;The Pin interrupt example demonstrates using the pin interrupt API functions&lt;BR /&gt;pin interrupts &amp;amp; wake up from low power sleep state using the pin&lt;BR /&gt;interrupts.&lt;/P&gt;&lt;P&gt;This example configures the pin interrupt channel 7 as falling edge&lt;BR /&gt;wake up interrupt. The interrupt channel 7 is connected to GPIO pin&lt;BR /&gt;PIO0-0 in GPIO block. The example will go to sleep mode. To wake up from&lt;BR /&gt;sleep mode, provide a falling edge pulse at GPIO pin PIO0-0.&lt;BR /&gt;On the LPCXpresso board, PIO0-0 is connected to pontentiometer which&lt;BR /&gt;can be used to provide falling edge pulse. The application will go to&lt;BR /&gt;sleep state in a loop, with every wake up the board LED0 will be toggled.&lt;/P&gt;&lt;P&gt;Special connection requirements&lt;BR /&gt;-------------------------------&lt;BR /&gt;The LPCXpresso base board is required with the LPCXpresso board to use this&lt;BR /&gt;example. The Manley board needs no extra hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 13:51:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-LPCopen-project-will-not-run-debug-LPC11U68-board/m-p/1264393#M44700</guid>
      <dc:creator>jDrum</dc:creator>
      <dc:date>2021-04-19T13:51:25Z</dc:date>
    </item>
    <item>
      <title>Re: Sample LPCopen project  will not run/debug LPC11U68 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-LPCopen-project-will-not-run-debug-LPC11U68-board/m-p/1265342#M44717</link>
      <description>&lt;P&gt;&lt;U&gt;Issue resolved&lt;/U&gt;.&amp;nbsp; The problem was that the USB cable was plugged into the target instead of the Link&lt;/P&gt;&lt;P&gt;&lt;U&gt;Alice&lt;/U&gt;: Thank you for your help in getting the board.h file issue resolved. (earlier post)&lt;/P&gt;&lt;P&gt;In general, the documentation supplied with the LTC11U68 board is completely useless for getting started.&amp;nbsp; (&lt;U&gt;12 years ago&lt;/U&gt; using the board for the LPC13xx was straight forward.&amp;nbsp; Was the LTCware site.)&lt;/P&gt;&lt;P&gt;1. The web address on the board box is incorrect.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; Locating the schematics was difficult.&amp;nbsp; Had to search using google instead of NXP.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp; No micro USB cable supplied.&amp;nbsp; Had to find one from an old tablet.&lt;/P&gt;&lt;P&gt;4.&amp;nbsp; Had to download the LPCopen software to even get started (I tried the MCUXpresso IDE first).&lt;/P&gt;&lt;P&gt;5. There are two USB connectors on the board.&amp;nbsp; Picking the one shown in the tutorial was incorrect.&amp;nbsp; The getting started should emphasize that Windows 10 will chime when the correct connector is used.&lt;/P&gt;&lt;P&gt;6.&amp;nbsp; We will need to do all of this again when the actual production PCB arrives.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Tue, 20 Apr 2021 19:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Sample-LPCopen-project-will-not-run-debug-LPC11U68-board/m-p/1265342#M44717</guid>
      <dc:creator>jDrum</dc:creator>
      <dc:date>2021-04-20T19:02:30Z</dc:date>
    </item>
  </channel>
</rss>