<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHigh clock rate of LPC1788-SPI performs error</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/High-clock-rate-of-LPC1788-SPI-performs-error/m-p/521832#M4468</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by qq on Wed Jul 22 00:20:04 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have configured an LPC1788 as SPI master on SSP1 (CPOL = 0; CPHA = 0) to communicate with a Nor Flash chip at 20 MHz.The Nor Flash chip needs the chip select pulled down (I do that with a GPIO), then a byte of command data need to be transmitted and some bytes of data need to be read and then the chip select needs to be pulled up again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I use Chip_SSP_WriteFrames_Blocking() function to send any data and the data does get transmitted and &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SSP_ReadFrames_Blocking () function to read any data from the Nor Flash accordingly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So everything's fine.However, As the frequency of the SSP for more than 20 MHz, the SSP can't work properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is: Why the SSP can't work properly more than 20 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:37:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:37:11Z</dc:date>
    <item>
      <title>High clock rate of LPC1788-SPI performs error</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/High-clock-rate-of-LPC1788-SPI-performs-error/m-p/521832#M4468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by qq on Wed Jul 22 00:20:04 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have configured an LPC1788 as SPI master on SSP1 (CPOL = 0; CPHA = 0) to communicate with a Nor Flash chip at 20 MHz.The Nor Flash chip needs the chip select pulled down (I do that with a GPIO), then a byte of command data need to be transmitted and some bytes of data need to be read and then the chip select needs to be pulled up again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I use Chip_SSP_WriteFrames_Blocking() function to send any data and the data does get transmitted and &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SSP_ReadFrames_Blocking () function to read any data from the Nor Flash accordingly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So everything's fine.However, As the frequency of the SSP for more than 20 MHz, the SSP can't work properly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is: Why the SSP can't work properly more than 20 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/High-clock-rate-of-LPC1788-SPI-performs-error/m-p/521832#M4468</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:37:11Z</dc:date>
    </item>
  </channel>
</rss>