<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 AN12327SW_Cannot run blhost.exe to connect the USB VCOM port</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN12327SW-Cannot-run-blhost-exe-to-connect-the-USB-VCOM-port/m-p/1262090#M44650</link>
    <description>&lt;P&gt;I use ConfigTools to add USB0 VCOM function into my LPC55S69. Then combine "dsbl" project.&lt;/P&gt;&lt;P&gt;I can connect the VCOM port by PuTTY or other simple tools, but cannot connect by using blhost.exe like command "blhost.exe -p COMxx,115200 get-property 1".&lt;/P&gt;&lt;P&gt;I found that in the callback function&lt;/P&gt;&lt;P&gt;"usb_status_t USB_DeviceInterface0CicVcomCallback(class_handle_t handle, uint32_t event, void *param)"&lt;/P&gt;&lt;P&gt;the parameter "acmReqParam-&amp;gt;setupValue" is always 0, which makes connection fail.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to make blhost.exe work by connecting USB VCOM port?&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 14:39:08 GMT</pubDate>
    <dc:creator>yenchuntung</dc:creator>
    <dc:date>2021-04-14T14:39:08Z</dc:date>
    <item>
      <title>AN12327SW_Cannot run blhost.exe to connect the USB VCOM port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN12327SW-Cannot-run-blhost-exe-to-connect-the-USB-VCOM-port/m-p/1262090#M44650</link>
      <description>&lt;P&gt;I use ConfigTools to add USB0 VCOM function into my LPC55S69. Then combine "dsbl" project.&lt;/P&gt;&lt;P&gt;I can connect the VCOM port by PuTTY or other simple tools, but cannot connect by using blhost.exe like command "blhost.exe -p COMxx,115200 get-property 1".&lt;/P&gt;&lt;P&gt;I found that in the callback function&lt;/P&gt;&lt;P&gt;"usb_status_t USB_DeviceInterface0CicVcomCallback(class_handle_t handle, uint32_t event, void *param)"&lt;/P&gt;&lt;P&gt;the parameter "acmReqParam-&amp;gt;setupValue" is always 0, which makes connection fail.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How to make blhost.exe work by connecting USB VCOM port?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 14:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/AN12327SW-Cannot-run-blhost-exe-to-connect-the-USB-VCOM-port/m-p/1262090#M44650</guid>
      <dc:creator>yenchuntung</dc:creator>
      <dc:date>2021-04-14T14:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: AN12327SW_Cannot run blhost.exe to connect the USB VCOM port</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/AN12327SW-Cannot-run-blhost-exe-to-connect-the-USB-VCOM-port/m-p/1262504#M44655</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;yenchuntung&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;blhost needs to be supported by MCUBOOT protocol. MCUBOOT protocol is supported by LPC55S69 BOOT ROM.&lt;/P&gt;
&lt;P&gt;LPC55S69 should run in ISP mode thus it can call MCUBOOT protocol to communicate with blhost.&lt;/P&gt;
&lt;P&gt;Your own developed USB VCOM port can't support blhost.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 05:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/AN12327SW-Cannot-run-blhost-exe-to-connect-the-USB-VCOM-port/m-p/1262504#M44655</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-04-15T05:49:13Z</dc:date>
    </item>
  </channel>
</rss>