<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Regarding to programing LPC1768</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261816#M44643</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think you can populate a standard 20 pins male JTAG connect on your PCB board with 100mil pitch, you can use J-Link or the other device to download/debug the board of LPC1768.&lt;/P&gt;
&lt;P&gt;This is the 20 pins JTAG connector pin assignment.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1618387731770.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142202i1F01CF249ED0CED2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1618387731770.png" alt="xiangjun_rong_0-1618387731770.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1618387731770.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 08:10:03 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-04-14T08:10:03Z</dc:date>
    <item>
      <title>Regarding to programing LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261700#M44636</link>
      <description>HI, I have designed a proto-type board for LPC1768 micro controller .I would like to know what are all the possible ways to program it for 1st time .</description>
      <pubDate>Wed, 14 Apr 2021 05:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261700#M44636</guid>
      <dc:creator>durga3887</dc:creator>
      <dc:date>2021-04-14T05:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding to programing LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261809#M44642</link>
      <description>&lt;P&gt;To program for the first time, you can use a debugger, connected via the SWD/JTAG port, or use FlashMagic to program via the USART.&lt;/P&gt;&lt;P&gt;For the debugger, you will need a debug probe, such as LPC-Link2 or the new MCU-Link, which cost about $15 each and to use the free MCUXpresso. You will also need the SWD circuit described here&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If you are going to write any code, having a debugger will save you a lot of time, so it is better to make sure you can use it from the start, rather than have to re-engineer you board to add it later.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 08:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261809#M44642</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-04-14T08:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding to programing LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261816#M44643</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I think you can populate a standard 20 pins male JTAG connect on your PCB board with 100mil pitch, you can use J-Link or the other device to download/debug the board of LPC1768.&lt;/P&gt;
&lt;P&gt;This is the 20 pins JTAG connector pin assignment.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1618387731770.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142202i1F01CF249ED0CED2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1618387731770.png" alt="xiangjun_rong_0-1618387731770.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;xiangjun_rong_0-1618387731770.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 08:10:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Regarding-to-programing-LPC1768/m-p/1261816#M44643</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-04-14T08:10:03Z</dc:date>
    </item>
  </channel>
</rss>