<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1768 Chain programming issue, in uVision using SEGGER</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-Chain-programming-issue-in-uVision-using-SEGGER/m-p/521826#M4462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rsameni on Mon Dec 02 12:26:44 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have customized board with two LPC1768, which pass data to each other via SPI. The problem I have is with their JTAG chain programming. When I program one of them the other one is also (usually) programmed; but the behavior is not very deterministic. I have all the recommended pull-ups and pull-downs required on the JTAG wires and the two MCU work with the same clock oscillator. Therefore, no additional seems to be required. I use the uVision Keil software + SEGGER for programming. SEGGER detects both devices on the chain and doesn't give any errors when I program them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've seen a rather old post on this, which was unanswered on SEGGER's forum: &lt;/SPAN&gt;&lt;A href="http://http://forum.segger.com/index.php?page=Thread&amp;amp;postID=5104#post5104"&gt;JTAG chain - 3 LPC1768 on board&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have a clue? Is there any special software setting required? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:52:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:52:07Z</dc:date>
    <item>
      <title>LPC1768 Chain programming issue, in uVision using SEGGER</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-Chain-programming-issue-in-uVision-using-SEGGER/m-p/521826#M4462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rsameni on Mon Dec 02 12:26:44 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have customized board with two LPC1768, which pass data to each other via SPI. The problem I have is with their JTAG chain programming. When I program one of them the other one is also (usually) programmed; but the behavior is not very deterministic. I have all the recommended pull-ups and pull-downs required on the JTAG wires and the two MCU work with the same clock oscillator. Therefore, no additional seems to be required. I use the uVision Keil software + SEGGER for programming. SEGGER detects both devices on the chain and doesn't give any errors when I program them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've seen a rather old post on this, which was unanswered on SEGGER's forum: &lt;/SPAN&gt;&lt;A href="http://http://forum.segger.com/index.php?page=Thread&amp;amp;postID=5104#post5104"&gt;JTAG chain - 3 LPC1768 on board&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone have a clue? Is there any special software setting required? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-Chain-programming-issue-in-uVision-using-SEGGER/m-p/521826#M4462</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:52:07Z</dc:date>
    </item>
  </channel>
</rss>