<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: lpc11u68 uart clrc663</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11u68-uart-clrc663/m-p/1260311#M44607</link>
    <description>&lt;P&gt;Hi, Roll,&lt;/P&gt;
&lt;P&gt;It appears that you requires the source code or library for the UART for LPC11U68, if it is the case, pls download the LPCopen package from the link, in includes the package based IAR, Keil and LPCXpresso tools.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 12 Apr 2021 07:17:32 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-04-12T07:17:32Z</dc:date>
    <item>
      <title>lpc11u68 uart clrc663</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11u68-uart-clrc663/m-p/1259731#M44589</link>
      <description>&lt;P&gt;Hi everyone.&amp;nbsp; I should have to read the UID value from a RFID reader (with CLRC663) chip using uart interface, with a LPC11u68jbd100 microcontroller. I now have the c language driver code for nxp of the spi interface and the serial port script driver code. Now we want the c language library for the serial port and example code. Thank you in advance for your attention and for what you'll do for me. Good work. Nice day.&lt;/P&gt;</description>
      <pubDate>Sat, 10 Apr 2021 07:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11u68-uart-clrc663/m-p/1259731#M44589</guid>
      <dc:creator>Roll</dc:creator>
      <dc:date>2021-04-10T07:09:57Z</dc:date>
    </item>
    <item>
      <title>Re: lpc11u68 uart clrc663</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11u68-uart-clrc663/m-p/1260311#M44607</link>
      <description>&lt;P&gt;Hi, Roll,&lt;/P&gt;
&lt;P&gt;It appears that you requires the source code or library for the UART for LPC11U68, if it is the case, pls download the LPCopen package from the link, in includes the package based IAR, Keil and LPCXpresso tools.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 12 Apr 2021 07:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc11u68-uart-clrc663/m-p/1260311#M44607</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-04-12T07:17:32Z</dc:date>
    </item>
  </channel>
</rss>