<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: Using 2 USB ports with LPC55S16-EVK</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1260175#M44600</link>
    <description>&lt;P&gt;This demo is for Keil and IAR. It doesn't support MCUXpresso IDE.&lt;/P&gt;</description>
    <pubDate>Mon, 12 Apr 2021 03:39:28 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-04-12T03:39:28Z</dc:date>
    <item>
      <title>Using 2 USB ports with LPC55S16-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1258661#M44565</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a LPC55S16-EVK, and my main goal is to connect 2 different machines to the EVK using USB ports.&lt;/P&gt;&lt;P&gt;1 machine connected to the USB Full-Speed port and 1 machine connected to the USB Hi-Speed port.&lt;/P&gt;&lt;P&gt;I need that both machines will detect the EVK as a USB device.&lt;/P&gt;&lt;P&gt;Currently, I'm able to detect the EVK as a USB device from my linux machine (connected to Full Speed USB port), using dev_composite_cdc_msc_bm exmaple.&lt;/P&gt;&lt;P&gt;Now, I would like to detect the Hi-Speed port as a USB device as well.&lt;/P&gt;&lt;P&gt;I'm looking for an example that uses both ports as USB devices.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 07:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1258661#M44565</guid>
      <dc:creator>embedded_eng_</dc:creator>
      <dc:date>2021-04-08T07:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Using 2 USB ports with LPC55S16-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1259346#M44581</link>
      <description>&lt;P&gt;&lt;SPAN&gt;embedded_eng_&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;As I know, MCUXpresso SDK doesn't include demo for dual USBs. MCUXpresso Config Tool can't configure two USBs either.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Our suggestion is to manually combine two existing MCUXpresso SDK USBs demos by user self.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;My colleague ever developed a demo code of USB device generic dual. see attached. Please note, we don't provide technical support for the code revise.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Apr 2021 04:54:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1259346#M44581</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-04-09T04:54:47Z</dc:date>
    </item>
    <item>
      <title>Re: Using 2 USB ports with LPC55S16-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1260041#M44593</link>
      <description>&lt;P&gt;Thanks for the replay.&lt;/P&gt;&lt;P&gt;I've tried to load this SDK to MCUXpresso without success.&lt;/P&gt;&lt;P&gt;I have installed the SDK:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2021-04-11 10-11-03.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141952iF371825D6C1DC3CE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot from 2021-04-11 10-11-03.png" alt="Screenshot from 2021-04-11 10-11-03.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then I clicked at "Import SDK example(s)" and could not find the dual USB one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also tried to click at "Import project(s) from file system" and select the SDK, but the "Projects" field is empty.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2021-04-11 10-40-11.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141957iDF2AB6D7ABF105D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot from 2021-04-11 10-40-11.png" alt="Screenshot from 2021-04-11 10-40-11.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I flash this Project to my board? and how can I modify the code?&lt;/P&gt;&lt;P&gt;(This is the first time I'm using this IDE..)&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Apr 2021 07:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1260041#M44593</guid>
      <dc:creator>embedded_eng_</dc:creator>
      <dc:date>2021-04-11T07:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: Using 2 USB ports with LPC55S16-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1260175#M44600</link>
      <description>&lt;P&gt;This demo is for Keil and IAR. It doesn't support MCUXpresso IDE.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Apr 2021 03:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-2-USB-ports-with-LPC55S16-EVK/m-p/1260175#M44600</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-04-12T03:39:28Z</dc:date>
    </item>
  </channel>
</rss>