<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC1768 doesn't start at power-up</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257290#M44532</link>
    <description>&lt;P&gt;Are you using the semihosting C library? If so, you need a debugger connected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try switching the C library to a NoHost version:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Switching-the-selected-C-library/m-p/473669" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Switching-the-selected-C-library/m-p/473669&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Apr 2021 11:19:38 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2021-04-06T11:19:38Z</dc:date>
    <item>
      <title>LPC1768 doesn't start at power-up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257250#M44531</link>
      <description>&lt;P&gt;I'm using a MCUXpresso to write software for a LPCXpresso1769 board. I've inserted code to blink the RGB led at startup in a distinct pattern.&lt;/P&gt;&lt;P&gt;I can compile and download the code to the board using the IDE, and I see the LED blink its pattern. However, I can't seem to get the board to run its code after power-up, without the help of the MCUXpresso IDE - it just sits there with the RGB LEDs colors lit up constantly.&lt;/P&gt;&lt;P&gt;How would I have to treat the board so that it runs the code I flashed onto it after power-on? I'm supplying power through the attached NP-Link board's micro-USB port.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Lena&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 10:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257250#M44531</guid>
      <dc:creator>Lena</dc:creator>
      <dc:date>2021-04-06T10:11:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 doesn't start at power-up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257290#M44532</link>
      <description>&lt;P&gt;Are you using the semihosting C library? If so, you need a debugger connected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Try switching the C library to a NoHost version:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Switching-the-selected-C-library/m-p/473669" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Switching-the-selected-C-library/m-p/473669&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 11:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257290#M44532</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-04-06T11:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1768 doesn't start at power-up</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257303#M44533</link>
      <description>&lt;P&gt;I set up the project again, and now it works. Strange, now we'll never find out what I did wrong ....&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 11:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1768-doesn-t-start-at-power-up/m-p/1257303#M44533</guid>
      <dc:creator>Lena</dc:creator>
      <dc:date>2021-04-06T11:45:15Z</dc:date>
    </item>
  </channel>
</rss>