<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SGPIO synchronizing as a slave device. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-synchronizing-as-a-slave-device/m-p/521817#M4453</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Nickel on Tue May 10 02:59:15 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi when used as a slave device it would seem the SGPIO has no mechanism to synchronize to the master device word / frame / LR clock. A bit of an oversight or have I missed something in the data sheet?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tried using a clock qualifier to gate the incoming clock to pull the data in line. This has mixed success and resync can take many frames.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a way to reset the POS counter from an input pin perhaps, much like a standard external SPI peripheral?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:39:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:39:01Z</dc:date>
    <item>
      <title>SGPIO synchronizing as a slave device.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-synchronizing-as-a-slave-device/m-p/521817#M4453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Nickel on Tue May 10 02:59:15 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi when used as a slave device it would seem the SGPIO has no mechanism to synchronize to the master device word / frame / LR clock. A bit of an oversight or have I missed something in the data sheet?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tried using a clock qualifier to gate the incoming clock to pull the data in line. This has mixed success and resync can take many frames.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a way to reset the POS counter from an input pin perhaps, much like a standard external SPI peripheral?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-synchronizing-as-a-slave-device/m-p/521817#M4453</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: SGPIO synchronizing as a slave device.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-synchronizing-as-a-slave-device/m-p/521818#M4454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-synchronizing-as-a-slave-device/m-p/521818#M4454</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:10:32Z</dc:date>
    </item>
  </channel>
</rss>