<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Need LPC2468 Drivers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-LPC2468-Drivers/m-p/1255760#M44495</link>
    <description>Does LPC24xx(LPC2468) controller has Device drivers???? Regards, Nandini</description>
    <pubDate>Thu, 01 Apr 2021 10:36:32 GMT</pubDate>
    <dc:creator>Nandini_19</dc:creator>
    <dc:date>2021-04-01T10:36:32Z</dc:date>
    <item>
      <title>Need LPC2468 Drivers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-LPC2468-Drivers/m-p/1255760#M44495</link>
      <description>Does LPC24xx(LPC2468) controller has Device drivers???? Regards, Nandini</description>
      <pubDate>Thu, 01 Apr 2021 10:36:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-LPC2468-Drivers/m-p/1255760#M44495</guid>
      <dc:creator>Nandini_19</dc:creator>
      <dc:date>2021-04-01T10:36:32Z</dc:date>
    </item>
    <item>
      <title>Re: Need LPC2468 Drivers</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-LPC2468-Drivers/m-p/1256003#M44509</link>
      <description>&lt;P&gt;Hi Nandini,&lt;/P&gt;
&lt;P&gt;You can find examples and drivers for this device in the Embedded Software section of this link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc2000-arm7/single-chip-16-bit-32-bit-micro-512-kb-flash-ethernet-can-isp-iap-usb-2-0-device-host-otg-external-memory-interface:LPC2468FBD208?tab=Design_Tools_Tab" target="_blank"&gt;Single-chip 16-bit/32-bit micro; 512 kB flash, Ethernet, CAN, ISP/IAP, USB 2.0 device/host/OTG, external memory interface | NXP Semiconductors&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Apr 2021 23:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-LPC2468-Drivers/m-p/1256003#M44509</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-04-01T23:03:01Z</dc:date>
    </item>
  </channel>
</rss>