<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NAND Flash with LPC55S16 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1253765#M44467</link>
    <description>&lt;P&gt;Hi Alexis,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the info.&lt;/P&gt;
&lt;P&gt;For NOR flash using SPI, is there any maximum memory size limit that can be interfaced with LPC?&lt;/P&gt;
&lt;P&gt;As per my understanding, external memory flash address are not mapped to microcontroller so there should be no size limit.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 29 Mar 2021 18:06:36 GMT</pubDate>
    <dc:creator>nxf64834</dc:creator>
    <dc:date>2021-03-29T18:06:36Z</dc:date>
    <item>
      <title>NAND Flash with LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1252088#M44431</link>
      <description>Hi,

Can we interface NAND Flash with LPC55S16? If yes, what is the maximum memory size that can be interfaced?
Also, what's the alternate for NAND flash which is compatible with LPC55S16?
There is no info available regarding this in datasheet or RM.

Thanks in advance!!</description>
      <pubDate>Thu, 25 Mar 2021 10:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1252088#M44431</guid>
      <dc:creator>nxf64834</dc:creator>
      <dc:date>2021-03-25T10:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash with LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1253080#M44453</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144747"&gt;@nxf64834&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The LPC55s16 doesn't have an external memory controller or SPIFI interface so the only memories supported will be the ones using SPI/I2C interface.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Sat, 27 Mar 2021 00:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1253080#M44453</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-03-27T00:20:53Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash with LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1253765#M44467</link>
      <description>&lt;P&gt;Hi Alexis,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the info.&lt;/P&gt;
&lt;P&gt;For NOR flash using SPI, is there any maximum memory size limit that can be interfaced with LPC?&lt;/P&gt;
&lt;P&gt;As per my understanding, external memory flash address are not mapped to microcontroller so there should be no size limit.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 18:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1253765#M44467</guid>
      <dc:creator>nxf64834</dc:creator>
      <dc:date>2021-03-29T18:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: NAND Flash with LPC55S16</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1254415#M44476</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/144747"&gt;@nxf64834&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;That's right, this will depend on the memory and how to commands are implemented.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 18:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/NAND-Flash-with-LPC55S16/m-p/1254415#M44476</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-03-30T18:32:59Z</dc:date>
    </item>
  </channel>
</rss>