<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC5516 ADC Channels in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1253517#M44464</link>
    <description>&lt;P&gt;As an alternate solution, what pins on the SWD are required for programming. Is the SWO pin required to program the LPC5516 over SWD interface? Is the SWCLK and SWDIO the only connections needed to program over the SWD?&lt;/P&gt;</description>
    <pubDate>Mon, 29 Mar 2021 10:12:06 GMT</pubDate>
    <dc:creator>adrian_lavin</dc:creator>
    <dc:date>2021-03-29T10:12:06Z</dc:date>
    <item>
      <title>LPC5516 ADC Channels</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1249805#M44384</link>
      <description>&lt;P&gt;We are using the LPC5516JBD64 which has eight ADC channels defined and want to use seven of them. Three of the channels share IO with the SWD interface. We would like to use the SWD to program the device at build time but after that use the IO as ADC inputs, Is there a recommended circuit configuration to allow this without using jumpers?&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 16:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1249805#M44384</guid>
      <dc:creator>adrian_lavin</dc:creator>
      <dc:date>2021-03-22T16:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516 ADC Channels</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1250255#M44394</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;It seems no, using jumper is easy method. &lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 08:51:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1250255#M44394</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-03-23T08:51:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516 ADC Channels</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1250349#M44398</link>
      <description>&lt;P&gt;From personal experience, I would recommend to avoid such configurations. You only barter for trouble.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 10:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1250349#M44398</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-03-23T10:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516 ADC Channels</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1253517#M44464</link>
      <description>&lt;P&gt;As an alternate solution, what pins on the SWD are required for programming. Is the SWO pin required to program the LPC5516 over SWD interface? Is the SWCLK and SWDIO the only connections needed to program over the SWD?&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 10:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1253517#M44464</guid>
      <dc:creator>adrian_lavin</dc:creator>
      <dc:date>2021-03-29T10:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC5516 ADC Channels</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1256932#M44528</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you do not use SWO tracing technology, this pin can not used as SWD interface.&lt;/P&gt;
&lt;P&gt;SWCLK, SWDIo and GND are necessary.&lt;/P&gt;
&lt;P&gt;About debug design, you can have a look at:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565&lt;/A&gt;&amp;nbsp; &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 03:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC5516-ADC-Channels/m-p/1256932#M44528</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-04-06T03:44:44Z</dc:date>
    </item>
  </channel>
</rss>