<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4088 SWO Tracing with CMSIS-DAP or J-Link in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-SWO-Tracing-with-CMSIS-DAP-or-J-Link/m-p/1253352#M44458</link>
    <description>&lt;P&gt;Hi, Christian,&lt;/P&gt;
&lt;P&gt;If you use SWO, you have to use SWD protocol(includinf SWDIO, SWCLK, SWO(optional)), the SWO pin of LPC4088 must be connected in the onboard CMSIS-DAP LPC-Link2 debugger and an external SEGGER J-Link probe.&lt;/P&gt;
&lt;P&gt;secondly, you have to use PRINTF() function in application code so that message in PRINT() function can output via SWO.&lt;/P&gt;
&lt;P&gt;I attach a doc which demos how to use SWO.&lt;/P&gt;
&lt;P&gt;Regarding the question where the PRINTF() function will output, it is dependent on the tools, the PRINT() function can output to console, uart, ITM.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Mon, 29 Mar 2021 06:00:54 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2021-03-29T06:00:54Z</dc:date>
    <item>
      <title>LPC4088 SWO Tracing with CMSIS-DAP or J-Link</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-SWO-Tracing-with-CMSIS-DAP-or-J-Link/m-p/1253060#M44451</link>
      <description>&lt;P&gt;I am trying to get SWO tracing inside MCUXpresso working. I have an LPC4088 QSB with the onboard CMSIS-DAP LPC-Link2 debugger and an external SEGGER J-Link probe.&lt;BR /&gt;&lt;BR /&gt;I can debug successfully with both probes, but when I start SWO tracing windows, its not possible to configure the SWO correctly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="swo_config.png" style="width: 494px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140789i42B640C045D64B34/image-dimensions/494x177?v=v2" width="494" height="177" role="button" title="swo_config.png" alt="swo_config.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What steps am I missing to get this to work with both probes?&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Fri, 26 Mar 2021 21:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-SWO-Tracing-with-CMSIS-DAP-or-J-Link/m-p/1253060#M44451</guid>
      <dc:creator>tux19</dc:creator>
      <dc:date>2021-03-26T21:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4088 SWO Tracing with CMSIS-DAP or J-Link</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-SWO-Tracing-with-CMSIS-DAP-or-J-Link/m-p/1253352#M44458</link>
      <description>&lt;P&gt;Hi, Christian,&lt;/P&gt;
&lt;P&gt;If you use SWO, you have to use SWD protocol(includinf SWDIO, SWCLK, SWO(optional)), the SWO pin of LPC4088 must be connected in the onboard CMSIS-DAP LPC-Link2 debugger and an external SEGGER J-Link probe.&lt;/P&gt;
&lt;P&gt;secondly, you have to use PRINTF() function in application code so that message in PRINT() function can output via SWO.&lt;/P&gt;
&lt;P&gt;I attach a doc which demos how to use SWO.&lt;/P&gt;
&lt;P&gt;Regarding the question where the PRINTF() function will output, it is dependent on the tools, the PRINT() function can output to console, uart, ITM.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 06:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4088-SWO-Tracing-with-CMSIS-DAP-or-J-Link/m-p/1253352#M44458</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-03-29T06:00:54Z</dc:date>
    </item>
  </channel>
</rss>