<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1759FBD80</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1759FBD80/m-p/1252781#M44445</link>
    <description>Hello, I am currently using the LPC1759FBD80 microcontroller to control 24 relays, I wonder if the outputs are on low state or high state at startup, or undetermined, because I do not want to excite the 24 relays at once I risk to burn out since the power is high with a total current of 2.4 Amp.</description>
    <pubDate>Fri, 26 Mar 2021 10:03:34 GMT</pubDate>
    <dc:creator>AMMOURKENZA1</dc:creator>
    <dc:date>2021-03-26T10:03:34Z</dc:date>
    <item>
      <title>LPC1759FBD80</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1759FBD80/m-p/1252781#M44445</link>
      <description>Hello, I am currently using the LPC1759FBD80 microcontroller to control 24 relays, I wonder if the outputs are on low state or high state at startup, or undetermined, because I do not want to excite the 24 relays at once I risk to burn out since the power is high with a total current of 2.4 Amp.</description>
      <pubDate>Fri, 26 Mar 2021 10:03:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1759FBD80/m-p/1252781#M44445</guid>
      <dc:creator>AMMOURKENZA1</dc:creator>
      <dc:date>2021-03-26T10:03:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1759FBD80</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1759FBD80/m-p/1253429#M44459</link>
      <description>&lt;P&gt;Peripheral in/outputs of basically all Cortex M devices are in a high-impedance state (Z) after startup or reset.&lt;/P&gt;&lt;P&gt;Peripheral units need to explicitly be enabled to work (power and clock).&lt;/P&gt;&lt;P&gt;To be safe, I would highly suggest to add pull-up or pull-down resistors to your relais drivers, to ensure startup in a safe state. The value should not interfere with the operation once the GPIO is enabled.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Mar 2021 08:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1759FBD80/m-p/1253429#M44459</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-03-29T08:16:00Z</dc:date>
    </item>
  </channel>
</rss>