<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CMSIS DAP UART and KEIL in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMSIS-DAP-UART-and-KEIL/m-p/1249985#M44390</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;How about this case now, yes, I think you can find help from KEIL support.&lt;/P&gt;</description>
    <pubDate>Tue, 23 Mar 2021 02:49:32 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2021-03-23T02:49:32Z</dc:date>
    <item>
      <title>CMSIS DAP UART and KEIL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMSIS-DAP-UART-and-KEIL/m-p/1238844#M44105</link>
      <description>&lt;P&gt;I'm using keil MDK to develop and I can debug with it and use the UART0 on the xpresso V2 board for the LPC11U68 - but only after I first run a debug session in LPCxpresso for this target and connect to it. Then, provided I keep the board powered and plugged into the link, I can stop LPCxpresso and start Keil with the CMSIS DAP selected as debugger and off I go. But Keil can't find the debugger from a power up of the board directly - and neither the debugger or the com port appear as devices to the (windows) computer that I'm running on.&lt;/P&gt;&lt;P&gt;Is there a way to cause the init of the debugger and serial port without using LPCxpresso to boot it?&lt;/P&gt;&lt;P&gt;I've also pinged ARM because this sounds like a driver issue in part (which is not the MCUXpresso fix if anyone is following that thread - it doesn't help).&lt;/P&gt;</description>
      <pubDate>Tue, 02 Mar 2021 18:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMSIS-DAP-UART-and-KEIL/m-p/1238844#M44105</guid>
      <dc:creator>ianholmes</dc:creator>
      <dc:date>2021-03-02T18:12:52Z</dc:date>
    </item>
    <item>
      <title>Re: CMSIS DAP UART and KEIL</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CMSIS-DAP-UART-and-KEIL/m-p/1249985#M44390</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;How about this case now, yes, I think you can find help from KEIL support.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 02:49:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CMSIS-DAP-UART-and-KEIL/m-p/1249985#M44390</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-03-23T02:49:32Z</dc:date>
    </item>
  </channel>
</rss>