<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: FAT filesystem for a external Flash</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/FAT-filesystem-for-a-external-Flash/m-p/1249876#M44386</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have FatFs using SPI implemented for this MCU, this is an issue with the SDK. I recommend you to check the following community document written by a colleague. The document is for Kinetis, however, the SD card operation based on the SPI is the same, you still can refer to it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Porting-FatFs-file-system-to-KL26-SPI-SD-card-code/ta-p/1111095" target="_blank" rel="noopener"&gt;Porting FatFs file system to KL26 SPI SD card code - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Mar 2021 19:16:13 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2021-03-22T19:16:13Z</dc:date>
    <item>
      <title>FAT filesystem for a external Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FAT-filesystem-for-a-external-Flash/m-p/1247145#M44311</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working with the LPCXpresso55s69 board using MCUXpresso and i have few problems with the File System middleware&lt;/P&gt;&lt;P&gt;I use an external flash connected through SPI as a USB MSD and i want to create and modify a file in the MSD with both pc and micro. The first one is not a problem but i'm wondering how to do it with the micro. I looked at the sdcard_fatfs_freertos example and i added to my project the file system components but files like&amp;nbsp;"fsl_sdspi_disk.h"&amp;nbsp;"fsl_nand_disk.h" are not found if the&amp;nbsp;SDSPI_DISK_ENABLE and NAND_DISK_ENABLE are enabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this the right way to procede? If so, why are these file not found? How can i add them to my project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much, have a great day&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 10:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FAT-filesystem-for-a-external-Flash/m-p/1247145#M44311</guid>
      <dc:creator>rd1</dc:creator>
      <dc:date>2021-03-17T10:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: FAT filesystem for a external Flash</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FAT-filesystem-for-a-external-Flash/m-p/1249876#M44386</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have FatFs using SPI implemented for this MCU, this is an issue with the SDK. I recommend you to check the following community document written by a colleague. The document is for Kinetis, however, the SD card operation based on the SPI is the same, you still can refer to it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Kinetis-Microcontrollers/Porting-FatFs-file-system-to-KL26-SPI-SD-card-code/ta-p/1111095" target="_blank" rel="noopener"&gt;Porting FatFs file system to KL26 SPI SD card code - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 19:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FAT-filesystem-for-a-external-Flash/m-p/1249876#M44386</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-03-22T19:16:13Z</dc:date>
    </item>
  </channel>
</rss>