<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC17xx using AHB_RAM_MEMORY for general purposes</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1249674#M44378</link>
    <description>&lt;P&gt;Thanks. My program does not use CAN, but as I can see, there is an address with memory size 0x800&lt;/P&gt;&lt;PRE&gt;0x40038000 0x0800&lt;/PRE&gt;&lt;P&gt;Could I use these RAM for general purpose like AHB?&lt;/P&gt;</description>
    <pubDate>Mon, 22 Mar 2021 12:35:33 GMT</pubDate>
    <dc:creator>castle</dc:creator>
    <dc:date>2021-03-22T12:35:33Z</dc:date>
    <item>
      <title>LPC17xx using AHB_RAM_MEMORY for general purposes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1225402#M43831</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to use AHB_RAM_MEMORY SRAM banks 0 and 1 as a general purpose ram. As I understand bank0 (&lt;SPAN class=""&gt;&lt;SPAN class="highlight selected"&gt;0x2007&lt;/SPAN&gt; C000 - &lt;SPAN class="highlight"&gt;0x2007&lt;/SPAN&gt; FFFF&lt;/SPAN&gt;) is used for USB and bank1 (&lt;SPAN class=""&gt;0x2008 0000 - 0x2008 3FFF&lt;/SPAN&gt;) is used for Ethernet.&lt;/P&gt;&lt;P&gt;Can I use Bank0 if my code does not implement any USB interface? Also, if my code uses Ethernet, can I use a part of Bank1 i.e. (&lt;SPAN class=""&gt;0x2008 2000 - 0x2008 3FFF&lt;/SPAN&gt;) of less? As I see at LPC17xx user manual, Ethernet uses (&lt;SPAN class=""&gt;0x2008 0000 - 0x2008 1FFF&lt;/SPAN&gt;). Please correct me if I am wrong.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 03 Feb 2021 09:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1225402#M43831</guid>
      <dc:creator>castle</dc:creator>
      <dc:date>2021-02-03T09:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx using AHB_RAM_MEMORY for general purposes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1226813#M43858</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SRAM is interfaced with the Advanced High-performance bus (AHB).&amp;nbsp; You can use it as generally purpose.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 05:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1226813#M43858</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-02-05T05:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx using AHB_RAM_MEMORY for general purposes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1226969#M43861</link>
      <description>&lt;P&gt;Just as a comment, you might want the review your projects's linker scripts and possible modify it to use of this RAM sections properly.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Feb 2021 08:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1226969#M43861</guid>
      <dc:creator>frank_m</dc:creator>
      <dc:date>2021-02-05T08:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx using AHB_RAM_MEMORY for general purposes</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1249674#M44378</link>
      <description>&lt;P&gt;Thanks. My program does not use CAN, but as I can see, there is an address with memory size 0x800&lt;/P&gt;&lt;PRE&gt;0x40038000 0x0800&lt;/PRE&gt;&lt;P&gt;Could I use these RAM for general purpose like AHB?&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 12:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC17xx-using-AHB-RAM-MEMORY-for-general-purposes/m-p/1249674#M44378</guid>
      <dc:creator>castle</dc:creator>
      <dc:date>2021-03-22T12:35:33Z</dc:date>
    </item>
  </channel>
</rss>