<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPc4357 uart problem</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249355#M44361</link>
    <description>&lt;P&gt;&lt;EM&gt;Hello&amp;nbsp;&lt;/EM&gt;&lt;SPAN&gt;&lt;EM&gt;XiangJun ,&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Thank you for your kind reply.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;As you told UART block is damaged.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;So I was wondering to know how even this possible that one pin getting damaged while all other ports are working as expected.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Is it the noise or power supply issue which can cause this?&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Because I was trying to add extra pullup across the RX pin though still its not working.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Another thing ,I &amp;nbsp; observed that , from RX to my ground pin the resistance should be around 5megaohm while it was working fine.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;But after it got damaged its resistance is decreased to around 450ohm.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;So If I &amp;nbsp; tried to add across the RX pin some resistor to bring it to same 5megaohm but still it didn't work for me.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Can you please clarify if anything or replacement is the only solution for above issue?&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;Thank &amp;amp; Regards,&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Ashrumochan&lt;/EM&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Mar 2021 06:10:11 GMT</pubDate>
    <dc:creator>Ashrumochan</dc:creator>
    <dc:date>2021-03-22T06:10:11Z</dc:date>
    <item>
      <title>LPc4357 uart problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249122#M44355</link>
      <description>&lt;P&gt;Hello Guys,&lt;BR /&gt;I am using two LPC4357 Microcontroller to establish uart protocol.&lt;BR /&gt;One card uart2 and other uart3.&lt;BR /&gt;I did all configuration and hardware connections and able to transmit and receive properly in both the cards. But all of a sudden Card 1 transmiiting but unable to receive.&lt;BR /&gt;I checked everythinh as I have not done any changes in software as well as hardware.&lt;BR /&gt;I could see the voltage at TX pin is 3.4v but at RX pin is 2.4v which feels like controller rx pin is driving low.&lt;/P&gt;&lt;P&gt;In other board both tx and rx pin have same voltage.&lt;BR /&gt;What might be the issue ?&lt;BR /&gt;I am able to load and debug anyway the other uart pins are working I checked except uart 2-&amp;gt; rx pin is behaving awkward.&lt;BR /&gt;&lt;BR /&gt;Can anybody suggest di need to replace the controller or anyway it can be get worked or how it happened like this?&lt;/P&gt;&lt;P&gt;Waiting for your quick response.&lt;/P&gt;</description>
      <pubDate>Sat, 20 Mar 2021 04:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249122#M44355</guid>
      <dc:creator>Ashrumochan</dc:creator>
      <dc:date>2021-03-20T04:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPc4357 uart problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249343#M44360</link>
      <description>&lt;P&gt;Hi, Ashrumochan,&lt;/P&gt;
&lt;P&gt;As you said that the Uart_Rx pin logic voltage is 2.4v, I think it is abnormal, if you unplug&amp;nbsp; the UART card, and test the UART card TX pin logic(the pin is not connected to the RX pin of LPC4357) , what is the logic voltage? If the UART card Tx logic voltage is 3.3V, after the pin is connected to RX pin of LPC4357, the logic voltage becomes to 2.4V, I suppose the UART of LPC4357 is damaged.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 05:49:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249343#M44360</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-03-22T05:49:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPc4357 uart problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249355#M44361</link>
      <description>&lt;P&gt;&lt;EM&gt;Hello&amp;nbsp;&lt;/EM&gt;&lt;SPAN&gt;&lt;EM&gt;XiangJun ,&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Thank you for your kind reply.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;As you told UART block is damaged.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;So I was wondering to know how even this possible that one pin getting damaged while all other ports are working as expected.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Is it the noise or power supply issue which can cause this?&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Because I was trying to add extra pullup across the RX pin though still its not working.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Another thing ,I &amp;nbsp; observed that , from RX to my ground pin the resistance should be around 5megaohm while it was working fine.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;But after it got damaged its resistance is decreased to around 450ohm.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;So If I &amp;nbsp; tried to add across the RX pin some resistor to bring it to same 5megaohm but still it didn't work for me.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Can you please clarify if anything or replacement is the only solution for above issue?&lt;/EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;Thank &amp;amp; Regards,&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Ashrumochan&lt;/EM&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 06:10:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249355#M44361</guid>
      <dc:creator>Ashrumochan</dc:creator>
      <dc:date>2021-03-22T06:10:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPc4357 uart problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249397#M44362</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Frankly speaking, I do not know why the Uart_RX pin is damaged, maybe the cause is noise, static charge...&lt;/P&gt;
&lt;P&gt;I suggest you add a ESD device on the Uart_Rx pin to protect the RX internal circuit.&lt;/P&gt;
&lt;P&gt;Currently, I suggest you replace the chip with a new one.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 06:54:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249397#M44362</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2021-03-22T06:54:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPc4357 uart problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249417#M44364</link>
      <description>&lt;P&gt;Thanks for your time and value added feedback.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ashrumochan&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 07:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPc4357-uart-problem/m-p/1249417#M44364</guid>
      <dc:creator>Ashrumochan</dc:creator>
      <dc:date>2021-03-22T07:08:28Z</dc:date>
    </item>
  </channel>
</rss>