<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55 USB host dual instance in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1246819#M44303</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Michael,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Currently, it is a limitation of the USB component to support one more instance of USB device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We are not able to provide the update of the USB component to support two USB devices in the MCUXpresso Config Tools at the moment&amp;nbsp; due to limited capacity.&lt;/P&gt;
&lt;P&gt;The only possible workaround is complete renaming of a generated USB code example (all files, global function and definitions) and generating a new one for the second USB device of the MCU. The shared definitions and USB device configuration must be merged.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
    <pubDate>Wed, 17 Mar 2021 03:54:00 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2021-03-17T03:54:00Z</dc:date>
    <item>
      <title>LPC55 USB host dual instance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1246612#M44297</link>
      <description>&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;We're actually working on a project using the two USB ports (HS/FS) of an LPC55S28 as host controllers.&lt;/P&gt;&lt;P&gt;When configuring both ports as host in MCUXpresso IDE, we get a message telling that only one host instance is allowed.&lt;/P&gt;&lt;P&gt;Could you please confirm there is no way to use the two ports as host with this USB library?&lt;/P&gt;&lt;P&gt;If yes, do you know any other USB stack capable to managing this configuration?&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 18:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1246612#M44297</guid>
      <dc:creator>Michael_25</dc:creator>
      <dc:date>2021-03-16T18:06:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 USB host dual instance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1246819#M44303</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Michael,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Currently, it is a limitation of the USB component to support one more instance of USB device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We are not able to provide the update of the USB component to support two USB devices in the MCUXpresso Config Tools at the moment&amp;nbsp; due to limited capacity.&lt;/P&gt;
&lt;P&gt;The only possible workaround is complete renaming of a generated USB code example (all files, global function and definitions) and generating a new one for the second USB device of the MCU. The shared definitions and USB device configuration must be merged.&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 03:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1246819#M44303</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-03-17T03:54:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55 USB host dual instance</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1622015#M52025</link>
      <description>&lt;P&gt;any news on 2x usb's running at the same time, i.e one host one device?&lt;/P&gt;</description>
      <pubDate>Sat, 25 Mar 2023 16:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55-USB-host-dual-instance/m-p/1622015#M52025</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2023-03-25T16:18:48Z</dc:date>
    </item>
  </channel>
</rss>