<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Drop in replacement for LPC546xx in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Drop-in-replacement-for-LPC546xx/m-p/1246554#M44296</link>
    <description>&lt;P&gt;The product I am working on uses an LPC54618J512ET180E. I noticed that recently, the LPC54628 was released and has the same TFBGA-180 package. From the datasheets it looks like the 54628 is a drop-in-replacement for the 54618. Is this true? If the pinout is the same, can I safely port software from the 54618 to the 54628 without needing to rewrite peripheral and IO drivers?&lt;/P&gt;&lt;P&gt;Additional information on the lifespan of the LPC54618J512ET180E package would be helpful as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Evan&lt;/P&gt;</description>
    <pubDate>Tue, 16 Mar 2021 15:57:46 GMT</pubDate>
    <dc:creator>evan_ohlsen</dc:creator>
    <dc:date>2021-03-16T15:57:46Z</dc:date>
    <item>
      <title>Drop in replacement for LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Drop-in-replacement-for-LPC546xx/m-p/1246554#M44296</link>
      <description>&lt;P&gt;The product I am working on uses an LPC54618J512ET180E. I noticed that recently, the LPC54628 was released and has the same TFBGA-180 package. From the datasheets it looks like the 54628 is a drop-in-replacement for the 54618. Is this true? If the pinout is the same, can I safely port software from the 54618 to the 54628 without needing to rewrite peripheral and IO drivers?&lt;/P&gt;&lt;P&gt;Additional information on the lifespan of the LPC54618J512ET180E package would be helpful as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Evan&lt;/P&gt;</description>
      <pubDate>Tue, 16 Mar 2021 15:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Drop-in-replacement-for-LPC546xx/m-p/1246554#M44296</guid>
      <dc:creator>evan_ohlsen</dc:creator>
      <dc:date>2021-03-16T15:57:46Z</dc:date>
    </item>
    <item>
      <title>Re: Drop in replacement for LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Drop-in-replacement-for-LPC546xx/m-p/1246903#M44307</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;". Is this true? "&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; Yes,LPC54628 is a drop-in-replacement for the LPC54618.&lt;/P&gt;
&lt;P&gt;"Additional information on the lifespan of the LPC54618J512ET180E"&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;gt; The longevity years of LPC546xx is 15, until Dec 2031.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1615962767062.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/139835i9847F12D7376260F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1615962767062.png" alt="Alice_Yang_0-1615962767062.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Mar 2021 06:32:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Drop-in-replacement-for-LPC546xx/m-p/1246903#M44307</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-03-17T06:32:53Z</dc:date>
    </item>
  </channel>
</rss>