<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flash a LPC5410x with mxli in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-a-LPC5410x-with-mxli/m-p/1245661#M44282</link>
    <description>&lt;P&gt;Hello dear NXP community, I would like to flash a bootloader on a LPC5410x with the mxli-3.3 tool from marc. The processor is recognised with the command ./mxli -n and output in the command line.&lt;/P&gt;&lt;P&gt;When trying to load a hex file onto the board, the error: Segmentation fault. I have read that errors can occur with hex files. So I tried to load a binary file. With the windows tool flash magic the loading worked without problems.&lt;/P&gt;&lt;P&gt;I tried to display some error causes with the following command:&lt;/P&gt;&lt;P&gt;./mxli -q -d/dev/ttyUSB0 -b115200 -c12M -g -v -k -i -x -E -T 10000 -p -G 3 LCS_Bootloader_Release.bin&lt;/P&gt;&lt;P&gt;The first partitions of the RAM were also successfully written:&lt;/P&gt;&lt;P&gt;Download to RAM [4096@0x02000000...&lt;/P&gt;&lt;P&gt;Download to RAM [4096@0x02001000...&lt;/P&gt;&lt;P&gt;Download to RAM [4096@0x02002000...&lt;/P&gt;&lt;P&gt;However, with RAM [4096@0x02003000... the errors came up:&lt;/P&gt;&lt;P&gt;ERROR: Data expected from LPC&lt;/P&gt;&lt;P&gt;ERROR: binary echo mismatch.&lt;/P&gt;&lt;P&gt;ERROR: write FLASH failed&lt;/P&gt;&lt;P&gt;Could someone perhaps give me a push in the right direction with this problem, or help me to find out where the problem is? I am grateful for any answer and help&lt;/P&gt;</description>
    <pubDate>Mon, 15 Mar 2021 10:55:07 GMT</pubDate>
    <dc:creator>tlint</dc:creator>
    <dc:date>2021-03-15T10:55:07Z</dc:date>
    <item>
      <title>Flash a LPC5410x with mxli</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-a-LPC5410x-with-mxli/m-p/1245661#M44282</link>
      <description>&lt;P&gt;Hello dear NXP community, I would like to flash a bootloader on a LPC5410x with the mxli-3.3 tool from marc. The processor is recognised with the command ./mxli -n and output in the command line.&lt;/P&gt;&lt;P&gt;When trying to load a hex file onto the board, the error: Segmentation fault. I have read that errors can occur with hex files. So I tried to load a binary file. With the windows tool flash magic the loading worked without problems.&lt;/P&gt;&lt;P&gt;I tried to display some error causes with the following command:&lt;/P&gt;&lt;P&gt;./mxli -q -d/dev/ttyUSB0 -b115200 -c12M -g -v -k -i -x -E -T 10000 -p -G 3 LCS_Bootloader_Release.bin&lt;/P&gt;&lt;P&gt;The first partitions of the RAM were also successfully written:&lt;/P&gt;&lt;P&gt;Download to RAM [4096@0x02000000...&lt;/P&gt;&lt;P&gt;Download to RAM [4096@0x02001000...&lt;/P&gt;&lt;P&gt;Download to RAM [4096@0x02002000...&lt;/P&gt;&lt;P&gt;However, with RAM [4096@0x02003000... the errors came up:&lt;/P&gt;&lt;P&gt;ERROR: Data expected from LPC&lt;/P&gt;&lt;P&gt;ERROR: binary echo mismatch.&lt;/P&gt;&lt;P&gt;ERROR: write FLASH failed&lt;/P&gt;&lt;P&gt;Could someone perhaps give me a push in the right direction with this problem, or help me to find out where the problem is? I am grateful for any answer and help&lt;/P&gt;</description>
      <pubDate>Mon, 15 Mar 2021 10:55:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-a-LPC5410x-with-mxli/m-p/1245661#M44282</guid>
      <dc:creator>tlint</dc:creator>
      <dc:date>2021-03-15T10:55:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flash a LPC5410x with mxli</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-a-LPC5410x-with-mxli/m-p/1245745#M44283</link>
      <description>&lt;P&gt;I suggest that you contact the author of the tool directly. You can find his email address from his website:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.windscooting.com/softy/mxli.html" target="_blank"&gt;http://www.windscooting.com/softy/mxli.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Mar 2021 13:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flash-a-LPC5410x-with-mxli/m-p/1245745#M44283</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-03-15T13:51:31Z</dc:date>
    </item>
  </channel>
</rss>