<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC58S28 USB Multilink fail to connect after writing the stack pointer register in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1242668#M44202</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I debuged my own board with PEMICRO Multilink and a LPC55s28 for months now without issues until I tried to change the address of the stack pointer by writing its register.&lt;/P&gt;&lt;P&gt;Code:&lt;BR /&gt;asm volatile("LDR R0, =0x20044000;");//Fin de SRAM4&lt;BR /&gt;asm volatile("MOV sp, R0;");&lt;BR /&gt;&lt;BR /&gt;I flashed the code and debug with success until I unplugged the Multilink.&lt;BR /&gt;Now I can't connect it again on my board.&lt;/P&gt;&lt;P&gt;I could reflashed the good code via ISP and Flash Magic, but iI still cannot connect the Multilink.&lt;/P&gt;&lt;P&gt;Is there a solution or must I replace the LPC55s28 ?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 09 Mar 2021 17:23:31 GMT</pubDate>
    <dc:creator>YodaC</dc:creator>
    <dc:date>2021-03-09T17:23:31Z</dc:date>
    <item>
      <title>LPC58S28 USB Multilink fail to connect after writing the stack pointer register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1242668#M44202</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I debuged my own board with PEMICRO Multilink and a LPC55s28 for months now without issues until I tried to change the address of the stack pointer by writing its register.&lt;/P&gt;&lt;P&gt;Code:&lt;BR /&gt;asm volatile("LDR R0, =0x20044000;");//Fin de SRAM4&lt;BR /&gt;asm volatile("MOV sp, R0;");&lt;BR /&gt;&lt;BR /&gt;I flashed the code and debug with success until I unplugged the Multilink.&lt;BR /&gt;Now I can't connect it again on my board.&lt;/P&gt;&lt;P&gt;I could reflashed the good code via ISP and Flash Magic, but iI still cannot connect the Multilink.&lt;/P&gt;&lt;P&gt;Is there a solution or must I replace the LPC55s28 ?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Mar 2021 17:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1242668#M44202</guid>
      <dc:creator>YodaC</dc:creator>
      <dc:date>2021-03-09T17:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC58S28 USB Multilink fail to connect after writing the stack pointer register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1243050#M44218</link>
      <description>&lt;P&gt;HI&lt;/P&gt;
&lt;P&gt;How does it connect if you create a NEW project under a NEW workspace in&lt;STRONG&gt; ISP mode&lt;/STRONG&gt;?&lt;/P&gt;
&lt;P&gt;How does it work if other debug probe for example LPC-Link2?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 07:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1243050#M44218</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-03-10T07:43:09Z</dc:date>
    </item>
    <item>
      <title>Re: LPC58S28 USB Multilink fail to connect after writing the stack pointer register</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1243288#M44226</link>
      <description>&lt;P&gt;Hi Jun Zhang,&lt;/P&gt;&lt;P&gt;I created a New Workspace and new project and it has worked.&lt;BR /&gt;Then I imported my own project and it has worked too.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;</description>
      <pubDate>Wed, 10 Mar 2021 13:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC58S28-USB-Multilink-fail-to-connect-after-writing-the-stack/m-p/1243288#M44226</guid>
      <dc:creator>YodaC</dc:creator>
      <dc:date>2021-03-10T13:07:50Z</dc:date>
    </item>
  </channel>
</rss>