<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN ROM Driver about LPC15xx series in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-ROM-Driver-about-LPC15xx-series/m-p/1238485#M44098</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a question about CAN in the LPC15xx series.&lt;/P&gt;&lt;P&gt;I use the ROM Driver Interface to create a send and receive program and check the operation.&lt;/P&gt;&lt;P&gt;There is only one CAN interrupt in NVIC.&lt;/P&gt;&lt;P&gt;Therefore, I understand that CAN interrupts are shared for transmission and reception.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to handle when CAN transmission and reception overlap?&lt;/P&gt;&lt;P&gt;I am worried that one of the communications will fail when the send and receive overlap.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;mountain777&lt;/P&gt;</description>
    <pubDate>Tue, 02 Mar 2021 07:16:16 GMT</pubDate>
    <dc:creator>mountain777</dc:creator>
    <dc:date>2021-03-02T07:16:16Z</dc:date>
    <item>
      <title>CAN ROM Driver about LPC15xx series</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-ROM-Driver-about-LPC15xx-series/m-p/1238485#M44098</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a question about CAN in the LPC15xx series.&lt;/P&gt;&lt;P&gt;I use the ROM Driver Interface to create a send and receive program and check the operation.&lt;/P&gt;&lt;P&gt;There is only one CAN interrupt in NVIC.&lt;/P&gt;&lt;P&gt;Therefore, I understand that CAN interrupts are shared for transmission and reception.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to handle when CAN transmission and reception overlap?&lt;/P&gt;&lt;P&gt;I am worried that one of the communications will fail when the send and receive overlap.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;mountain777&lt;/P&gt;</description>
      <pubDate>Tue, 02 Mar 2021 07:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/CAN-ROM-Driver-about-LPC15xx-series/m-p/1238485#M44098</guid>
      <dc:creator>mountain777</dc:creator>
      <dc:date>2021-03-02T07:16:16Z</dc:date>
    </item>
  </channel>
</rss>