<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: UART with High Baud Rate [LPC1788]</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521773#M4409</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gjzxwht on Sat May 17 02:41:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;chip error&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 16:36:38 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T16:36:38Z</dc:date>
    <item>
      <title>UART with High Baud Rate [LPC1788]</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521771#M4407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by crudo on Mon Jul 15 15:26:29 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying use the LPC1788 UART with baud rate greater than 115200 bps, but without success.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;To control the UART I'm using the PDL (peripheral driver library), all work fine to baud rates up to 115200, with baud rate = 230400, for example, I get the followings errors on line status: FE (frame error), BI (break interrupt), RXFE (RX FIFO error). The baud rate error is lower than 2%, so I don't think that is the problem. Any sugestion about this trouble?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521771#M4407</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: UART with High Baud Rate [LPC1788]</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521772#M4408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by embd02161991 on Thu Aug 15 14:53:06 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Crudo ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Frame error occurs when the character in RXDAT was received with a missing stop bit at the expected location. This could be an indication of a baud rate or configuration mismatch with the transmitting source. If software needs to change the baud rate, the following sequence should be used: 1) Make sure the USART is not currently sending or receiving data. 2) Disable the USART by writing a 0 to the Enable bit (0 may be written to the entire registers). 3) Write the new BRGVAL. 4) Write to the CFG register to set the Enable bit to 1. I think this should help !&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SK&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:36:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521772#M4408</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:36:38Z</dc:date>
    </item>
    <item>
      <title>Re: UART with High Baud Rate [LPC1788]</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521773#M4409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gjzxwht on Sat May 17 02:41:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;chip error&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 16:36:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART-with-High-Baud-Rate-LPC1788/m-p/521773#M4409</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T16:36:38Z</dc:date>
    </item>
  </channel>
</rss>