<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックTCP/IP server under cpp with LPC4088</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/TCP-IP-server-under-cpp-with-LPC4088/m-p/1237861#M44088</link>
    <description>&lt;P&gt;Hello together,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to program a TCP/IP Server with an LPC4088 under cpp and I want to use the lwip library.&lt;/P&gt;&lt;P&gt;When I try the c-example of the lwio lib the echo-server works fine. If I alter the example to work for cpp the mcu doesn't even get an IP from the router.&lt;/P&gt;&lt;P&gt;Does anyone have a solution for this or a server example that works for cpp?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 09:22:53 GMT</pubDate>
    <dc:creator>CSeemann</dc:creator>
    <dc:date>2021-03-01T09:22:53Z</dc:date>
    <item>
      <title>TCP/IP server under cpp with LPC4088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TCP-IP-server-under-cpp-with-LPC4088/m-p/1237861#M44088</link>
      <description>&lt;P&gt;Hello together,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I try to program a TCP/IP Server with an LPC4088 under cpp and I want to use the lwip library.&lt;/P&gt;&lt;P&gt;When I try the c-example of the lwio lib the echo-server works fine. If I alter the example to work for cpp the mcu doesn't even get an IP from the router.&lt;/P&gt;&lt;P&gt;Does anyone have a solution for this or a server example that works for cpp?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Chris&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 09:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TCP-IP-server-under-cpp-with-LPC4088/m-p/1237861#M44088</guid>
      <dc:creator>CSeemann</dc:creator>
      <dc:date>2021-03-01T09:22:53Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP server under cpp with LPC4088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/TCP-IP-server-under-cpp-with-LPC4088/m-p/1237986#M44092</link>
      <description>&lt;P&gt;If you are using C++, don't forget to use extern "C" for the interrupt handlers.&lt;/P&gt;&lt;P&gt;&lt;A href="https://embeddedartistry.com/blog/2017/05/01/mixing-c-and-c-extern-c/" target="_blank"&gt;https://embeddedartistry.com/blog/2017/05/01/mixing-c-and-c-extern-c/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 13:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/TCP-IP-server-under-cpp-with-LPC4088/m-p/1237986#M44092</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-03-01T13:55:51Z</dc:date>
    </item>
  </channel>
</rss>