<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 What is the recommended microcontroller series that replaces the LPC1768 series?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/1237759#M44082</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Anyone please suggest exact pin to pin replacement for LPC17xx series.&lt;/P&gt;&lt;P&gt;I have existing designs, modify hardware is a problem, but I have a lot of code (tons) using LPC2148 peripherals (UART, I2C, Timers, ...), which new family is peripheral-software compatible?.&lt;/P&gt;&lt;P&gt;What series recommended for new designs has roughly equivalent capability (Memory size, speed, peripherals, etc.)?&lt;/P&gt;</description>
    <pubDate>Mon, 01 Mar 2021 06:58:20 GMT</pubDate>
    <dc:creator>Applied123</dc:creator>
    <dc:date>2021-03-01T06:58:20Z</dc:date>
    <item>
      <title>What is the recommended microcontroller series that replaces the LPC1768 series?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/1237759#M44082</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Anyone please suggest exact pin to pin replacement for LPC17xx series.&lt;/P&gt;&lt;P&gt;I have existing designs, modify hardware is a problem, but I have a lot of code (tons) using LPC2148 peripherals (UART, I2C, Timers, ...), which new family is peripheral-software compatible?.&lt;/P&gt;&lt;P&gt;What series recommended for new designs has roughly equivalent capability (Memory size, speed, peripherals, etc.)?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 06:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/1237759#M44082</guid>
      <dc:creator>Applied123</dc:creator>
      <dc:date>2021-03-01T06:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: What is the recommended microcontroller series that replaces the LPC1768 series?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/1237781#M44084</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;the LPC1768 is a replacement for the LPC2368. and the LPC1769 is a replacement for the LPC1768. The only difference is the max clock frequency (120Mhz) . A replacement with less memory is the LPC1766.LPC4078 is an option for LPC176x replacement.(&lt;A href="http://www.nxp.com/products/microcontrollers/core/cortex_m4_m4f/LPC4078FBD100.html" target="_blank"&gt;http://www.nxp.com/products/microcontrollers/core/cortex_m4_m4f/LPC4078FBD100.html&lt;/A&gt; )&lt;BR /&gt;Please note LPC4078 release time is 2013, 15 years longevity.&lt;/P&gt;
&lt;P&gt;Our Recommendation is LPC546xx or LPC540xx MCUs series, based on Cortex M4 core at 220MHz (with optional secondary Cortex M0+ core), similar peripherals, up to 512KB Flash and up to 200KB RAM.Please check more information in the following link:&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc54000-series-cortex-m4-mcus:MC_1414576688124" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc54000-series-cortex-m4-mcus:MC_1414576688124&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;LPC546xx and LPC540xx are not pin to pin replacement of LPC17xx&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a nice day,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 07:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/1237781#M44084</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2021-03-01T07:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: What is the recommended microcontroller series that replaces the LPC1768 series?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/2170370#M58767</link>
      <description>&lt;P&gt;I have the same question, and appreciate it's now almost 5 years later.&lt;/P&gt;&lt;P&gt;Which series of microcontrollers should I be looking at to use for new designs?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Sep 2025 10:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-is-the-recommended-microcontroller-series-that-replaces-the/m-p/2170370#M58767</guid>
      <dc:creator>jonathansmith</dc:creator>
      <dc:date>2025-09-16T10:04:17Z</dc:date>
    </item>
  </channel>
</rss>