<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Reading the ECRP level using the ISP-AP in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-the-ECRP-level-using-the-ISP-AP/m-p/1237425#M44072</link>
    <description>&lt;P&gt;I want to read the ECRP protection level of an LPC54628.&amp;nbsp; The user manual UM10912 section 49.6.4 says the ISP-AP is active no matter what ECRP level is set. Table 1078 describes the ISP-AP command "Query ECRP Level" which presumably returns the relevant bits I need.&lt;/P&gt;&lt;P&gt;Can anyone describe how to execute this ISP-AP command using a J-Link or Link-2 debugger and how the data is returned?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Feb 2021 19:02:20 GMT</pubDate>
    <dc:creator>jking1</dc:creator>
    <dc:date>2021-02-26T19:02:20Z</dc:date>
    <item>
      <title>Reading the ECRP level using the ISP-AP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-the-ECRP-level-using-the-ISP-AP/m-p/1237425#M44072</link>
      <description>&lt;P&gt;I want to read the ECRP protection level of an LPC54628.&amp;nbsp; The user manual UM10912 section 49.6.4 says the ISP-AP is active no matter what ECRP level is set. Table 1078 describes the ISP-AP command "Query ECRP Level" which presumably returns the relevant bits I need.&lt;/P&gt;&lt;P&gt;Can anyone describe how to execute this ISP-AP command using a J-Link or Link-2 debugger and how the data is returned?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 19:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Reading-the-ECRP-level-using-the-ISP-AP/m-p/1237425#M44072</guid>
      <dc:creator>jking1</dc:creator>
      <dc:date>2021-02-26T19:02:20Z</dc:date>
    </item>
  </channel>
</rss>